Heat Pump Thermostat Guide: How They Work, Features, Settings

By Ryan Mayes
Expert Review By Janet Shaw | Product Manager, Thermostats
September 30, 2026

A heat pump thermostat is a specialized climate control device designed to manage the unique heating and cooling cycles of a heat pump system. By continuously monitoring indoor conditions, a heat pump thermostat dictates when the compressor runs, when the reversing valve engages, and when auxiliary heating sources are activated.

A modern heat pump thermostat acts as the brain of your HVAC system, optimizing your home for energy efficiency while benefiting the people inside. It seamlessly bridges the gap between ambitious sustainability goals and practical, everyday comfort.

a heat pump smart thermostat sits installed in entryway a heat pump smart thermostat sits installed in entryway

How Does A Heat Pump Thermostat Differ From A Standard Thermostat?

A heat pump thermostat differs from a standard thermostat primarily through its ability to control a reversing valve and manage auxiliary heating systems. While standard thermostats only send simple on/off signals to a furnace or air conditioner, a heat pump thermostat must coordinate multiple heating stages and defrost cycles.

When a heat pump switches from cooling to heating, it relies on a reversing valve to change the flow of refrigerant. A heat pump thermostat is specifically wired with an "O" or "B" terminal to control this valve. Standard thermostats lack these specific terminals and the internal logic required to trigger this reversal.

Furthermore, heat pumps often rely on secondary heat sources, such as electric resistance coils, during extreme cold snaps. A heat pump thermostat intelligently decides when to activate this emergency or auxiliary heat to maintain comfort without wasting energy. A standard thermostat is completely unequipped to manage this delicate balance, which can result in the auxiliary heat running constantly and driving up utility costs.

Why Is A Specialized Heat Pump Thermostat Essential For Energy Efficiency?

A specialized heat pump thermostat is essential for energy efficiency because it prevents the unnecessary activation of high-cost auxiliary heating systems. By using advanced algorithms to maximize the use of the primary heat pump compressor, it significantly reduces electricity consumption.

Energy efficiency is the cornerstone of a sustainable, intelligent home. Heat pumps are incredibly efficient when operating in their primary mode, transferring ambient heat from the outside air into your home. Learn more about how a heat pump works. However, if the temperature drops drastically, the system needs help. A smart heat pump thermostat calculates the exact moment auxiliary heat is necessary, rather than turning it on at the first sign of a temperature drop.

How Does A Heat Pump Thermostat Control Auxiliary Heat?

A heat pump thermostat controls auxiliary heat by utilizing a process called "staging," which measures the gap between the current room temperature and the target setpoint. If the heat pump alone cannot close this temperature gap within a specific timeframe, the thermostat automatically engages the auxiliary heat to make up the difference.

Auxiliary heat (often electric resistance strips or a backup gas furnace) is a secondary heating stage designed to assist the heat pump during freezing weather. The heat pump thermostat constantly monitors the outdoor temperature and the indoor heating progress. If the indoor temperature falls two to three degrees below the setpoint, the thermostat signals the auxiliary heat to turn on.

Once the indoor temperature approaches the target, the heat pump thermostat shuts off the auxiliary heat and allows the highly efficient heat pump compressor to maintain the climate. This precise control mechanism keeps people comfortable while aggressively protecting against energy waste. Advanced models even allow users to set an "auxiliary lockout temperature," preventing the backup heat from turning on at all if the outdoor weather is relatively mild.

What Smart Features Should You Look For In A Heat Pump Thermostat?

When selecting a heat pump thermostat, you should look for thermostat benefits like adaptive recovery, Wi-Fi connectivity, geofencing, and learning algorithms. These intelligent capabilities transform a basic temperature dial into a comprehensive home energy management system.

Adaptive recovery (also known as smart recovery) is a crucial feature for heat pumps. It allows the heat pump thermostat to learn exactly how long your system takes to heat or cool your home. Instead of blasting expensive auxiliary heat to reach a set temperature quickly, the thermostat slowly ramps up the primary heat pump compressor in advance, saving significant energy.

Other visionary features defining the market in 2026 include:

  • Wi-Fi Connectivity: Allows homeowners to control their heat pump thermostat remotely via smartphone apps, ensuring comfort is always at their fingertips.
  • Geofencing: Uses your phone’s location to automatically adjust the temperature when you leave or return home, optimizing energy use without manual input.
  • Learning Algorithms: Automatically adapts to your daily schedule and temperature preferences, creating a custom heating and cooling profile over time.
  • Energy Reports: Provides detailed analytics on your HVAC usage, empowering you to make data-driven decisions about your home's energy consumption.
  • Voice Control: Integrates seamlessly with smart home ecosystems like Amazon Alexa, Google Assistant, or Apple HomeKit for hands-free adjustments.

Check out Carrie’s wide array of thermostats to help determine the best smart thermostat for your home.

What Are The Best Temperature Settings For A Heat Pump Thermostat?

The best temperature settings for a heat pump thermostat are 68°F (20°C) during the winter and 78°F (25°C) during the summer while you are awake and at home. Setting your heat pump thermostat to these industry-recommended baselines maximizes energy savings while maintaining a comfortable indoor environment.

Unlike traditional gas furnaces, heat pumps operate best when maintaining a steady temperature. Drastic temperature setbacks—such as lowering the heat by 10 degrees at night—can actually waste money. When the heat pump thermostat tries to recover from a deep temperature drop the next morning, it is often forced to rely on expensive auxiliary heat.

Instead, experts recommend a "set it and forget it" approach, or using very mild setbacks of only two to three degrees when sleeping or away. A smart heat pump thermostat with adaptive recovery is better suited for teams and families that prefer automated temperature changes, while a manual heat pump thermostat works best when kept at a consistent, comfortable baseline throughout the day.

Learn more in our guide on what temperature should I set my thermostat?

carrier what temperature should i set my thermostat infographic carrier what temperature should i set my thermostat infographic

Frequently Asked Questions

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

About The Author: Janet Shaw is a Product Manager for Residential Thermostats at Carrier Corporation, where she focuses on developing innovative thermostat solutions that help homeowners improve comfort, convenience, and energy efficiency. Janet's goal is to help consumers better understand smart thermostat technology so they can make informed decisions about managing their home's comfort.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.