Gas vs. Electric vs. Oil: Comparing Types of Furnaces
When comparing a gas vs electric furnace—or considering an oil furnace—the best choice depends on your climate, fuel availability, and long-term budget. Gas furnaces offer powerful heating for cold regions, electric furnaces provide quiet, low-maintenance operation for milder climates, and oil furnaces deliver intense heat where gas lines aren't available.
With more choices than ever when buying a new furnace, the decision usually starts with the fuel source. No matter which type fits your home, there’s a furnace designed to meet your needs for comfort and efficiency.
Gas vs Electric Furnace
A gas furnace uses natural gas to create a flame that heats the air, making it ideal for freezing temperatures, while an electric furnace uses heating coils, similar to a hair dryer, making it better for moderate climates.
The gas vs electric furnace comparison obviously starts with fuel source, but there are significant differences in furnace installation, operating costs, and expected lifespan.
Efficiency and Climate Suitability
Natural gas furnaces typically heat the home faster because they generate warm air at higher temperatures than an electrical heat system. Because natural gas costs are generally lower than electricity rates, these furnaces are best suited for colder, northern climates where the heating season is longer and more intense.
Installation and Maintenance
When looking at electric furnace vs gas models, electric units often have the advantage in upfront simplicity. Electric furnaces don’t require venting systems or gas hookups and can cost less to purchase and install. Gas furnaces require more standard furnace maintenance, so those costs will be higher. However, electric units are often quieter and can last longer due to fewer moving parts.
Gas vs Oil Heating
Oil furnace vs gas heating often comes down to infrastructure: gas requires a pipeline connection, while oil requires a storage tank but can be delivered anywhere.
For rural areas and older neighborhoods where natural gas pipelines aren't available, oil heating is a robust option. Both use internal combustion to create heat, making them effective for colder climates.
Cost and Convenience
Natural gas furnaces typically have lower initial costs for the furnace itself. However, the gas is supplied through a pipeline infrastructure, which is a limiting factor for some homeowners.
Oil burning furnaces convert more heat per BTU than other heating sources. However, they typically have slightly lower AFUE efficiency ratings than natural gas models. They also require a storage tank for fuel, which can add cost to an oil furnace installation.
Maintenance Needs
Both types require regular upkeep, but gas furnaces avoid the soot and dirt buildup common in oil furnaces, which can add time and cost for professional cleaning.
Oil Furnace vs Electric Furnace Cost
In an electric vs oil furnace comparison, oil furnaces generally have higher upfront costs due to equipment and fuel tanks, but they heat homes much faster in extreme cold than electric resistance heating.
Upfront Investment
Average cost, including furnace installation, is more for an oil furnace compared to electric. If you need to install a tank for fuel oil, add roughly two thousand dollars to that total cost. Both types are often installed as central, forced air systems. Learn more about the cost of a furnace.
Comfort and Operating Costs
Fuel oil heated homes heat up faster because oil furnaces create higher temperatures. This makes oil a better choice for cold climates, while electric furnaces are commonly used in warmer climates with less heating demand. Long-term costs fluctuate more with oil.
Benefits Overview for Types of Furnaces
When we compare gas vs oil vs electric furnaces, there is no single winner. The best fit matches your climate, expectations for comfort, and local fuel sources.
Gas Furnaces
Benefits
- Lower fuel costs
- High energy efficiency / low operating costs
- Warmer heating temperatures for colder climates
- No fuel tank needed
Disadvantages
- Requires pipeline infrastructure
- Installation requires outside venting and gas hookup
- Potential for natural gas leak or CO infiltration
Oil Furnaces
Benefits
- Generates more heat per BTU than natural gas
- Fuel oil can be delivered to remote areas without gas lines
Disadvantages
- Higher first cost for the furnace
- Higher fuel oil prices and volatility
- Lower energy efficiency (AFUE) than gas
- Needs more maintenance due to soot buildup
Electric Furnaces
Benefits
- Lower initial cost for furnace & installation
- Longer average lifespan
- Quiet operation
- No potentially harmful gas byproducts
Disadvantages
- Generates lower heating temperatures
- Less capable in severe cold
- High operating costs despite high AFUE ratings (electricity is often more expensive than gas)
What is a Forced Air Furnace?
You may hear the term "forced air furnace" when comparing models. This simply refers to a heating system that uses a fan or blower to circulate warm air through ducts. Whether you choose a gas vs electric furnace or an oil model, most modern residential systems are considered forced air.
Let A Carrier Expert Weigh In On Furnace Type
Still deciding between electric vs oil furnace options or gas models? Carrier has you covered. We offer a comprehensive family of furnaces and a nationwide network of experts to help you determine the right type of furnace for your home. Find a local Carrier expert today.
Frequently Asked Questions
Whether a gas vs electric furnace is better depends on your location. Gas furnaces are generally superior for cold climates due to higher heat output and lower fuel costs. Electric furnaces are better for moderate climates where winters are mild, offering lower upfront costs and easier maintenance.
If you want to reduce your carbon footprint, electric heating can be greener, especially if powered by renewable energy. However, consider the higher operating costs associated with electric heat and the availability of natural gas in your area. It's advisable to evaluate long-term costs, energy efficiency, and personal preferences before making the switch.
Heating a house with gas is typically cheaper than using electricity, as natural gas prices are usually lower than electricity rates. Gas furnaces also tend to be more efficient in converting energy into heat, leading to lower overall heating costs.
The main downsides include higher monthly operating bills and slower heating times compared to gas or oil. Additionally, electric furnaces rely entirely on the grid, making you vulnerable to power outages during winter storms unless you have a backup generator.
Electric furnaces typically last the longest—often 20 to 30 years—because they have fewer moving parts and do not involve combustion. Gas and oil furnaces generally last between 15 and 20 years with proper maintenance.
No. Electric furnaces do not create exhaust and do not need a chimney or vent. Gas and oil furnaces burn fuel and require proper venting to the outdoors to safely expel byproducts like carbon monoxide.
About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.