How Many Carbon Monoxide Detectors Do I Need?

By Travis Baugh

You need at least one carbon monoxide (CO) detector on every level of your home, including the basement. Additionally, you should install detectors inside or directly outside every sleeping area to ensure alarms wake you up. For maximum safety, place a detector 15–20 feet away from every fuel-burning appliance, such as a furnace or garage.

Quick Summary: CO Detector Requirements

  • Per Floor: One on every level (including basements).
  • Sleeping Areas: One inside or near every bedroom.
  • Appliances: One 15–20 feet from fuel-burning sources (furnace, fireplace, water heater).
  • Garages: One near (not inside) attached garages.
how many carbon monoxide detectors do i need infographic how many carbon monoxide detectors do i need infographic

Detailed Guide to Carbon Monoxide Detector Placement

Determining exactly how many carbon monoxide detectors should be in a home depends on your layout and the fuel-burning equipment you use. While a single detector is better than nothing, it is rarely enough to protect an entire household from this odorless, colorless gas.

 1. One Detector on Every Level

Gas is slightly lighter than air and diffuses evenly throughout a room. To catch rising levels early, it is strongly recommended that you install a carbon monoxide detector on every story of your home. If you have a two-story home with a basement, that means you need a minimum of three detectors.

2. Coverage for Sleeping Areas

Carbon monoxide poisoning is most dangerous when you are asleep because the gas can incapacitate you before you wake up.

  • Best Practice: Install a detector inside every bedroom, especially if the room contains a gas or propane furnace.
  • Minimum Requirement: Install detectors in the hallway outside sleeping areas so the alarm is loud enough to be clearly heard through closed doors.

3. Placement Near Fuel-Burning Sources

Fuel-burning appliances are potential sources of CO leaks. Place detectors near:

  • Gas furnaces
  • Gas water heaters
  • Fireplaces
  • Gas stoves
  • Attached garages (car emissions)

Critical Tip: Keep detectors at least 15 feet away from these appliances. Placing them too close can cause false alarms from small, safe puffs of combustion gas during startup.

Why Do I Need a Carbon Monoxide Detector?

You need carbon monoxide detectors because CO is impossible to detect with human senses—you cannot see it, smell it, or taste it. Without a detector, dangerous buildup from malfunctioning equipment like furnaces, stoves, or generators can lead to poisoning.

To help prevent dangerous CO levels:

  • Install Detectors: This is your first line of defense.
  • Ventilation: Keep vents clear around fuel-burning devices.
  • Maintenance: Have your HVAC system and gas/oil/coal equipment serviced annually by a qualified technician.
  • Garage Safety: Never run a car inside an attached garage, even with the door open.
  • Proper Use: Never use generators or charcoal grills indoors.
how many carbon monoxide detectors do i need how many carbon monoxide detectors do i need

Maintaining Your Carbon Monoxide Detectors

Proper maintenance ensures your detectors are ready to protect your family. Once installed, follow these steps:

  1. Test Regularly: Use the "test" button to ensure the battery and sensor are functioning.
  2. Clean Monthly: Vacuum the detector to remove dust that might clog the sensor. Note: Do not use chemicals or solvents.
  3. Check Location: Ensure furniture or curtains aren't blocking the sensor.
  4. Replace as Needed: CO detectors have a lifespan (usually 5–7 years); replace them before they expire.

Learn more about the best carbon monoxide detector placement.

Connect With a Carrier Dealer

Still unsure how many carbon monoxide detectors do I need for your specific layout? Your local Carrier dealer can assess your home and recommend the right safety solutions. Schedule an appointment today to secure your peace of mind.

graphic shows features of carrier carbon monoxide alarm graphic shows features of carrier carbon monoxide alarm

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.