Skip to main content

VIND EEN DEALER

CONTACT

carrier-case-study-crashed-ice-event-ice-track-at-night_h

Red Bull Crashed Ice event

Carrier Rental Systems supplied high efficiency chillers and defrost boilers for the downhill ice track at the Red Bull Crashed Ice event in Belfast.
carrier-map-case-study-uk
account_circleCustomer AST Eistechnik
roomLocation Belfast, United Kingdom
todayDate 2015
carrier-case-study-crashed-ice-event-air-cooled-chiller-30RB

Project description

Carrier Rental Systems, one of the UK's leading temporary cooling and heating specialists, delivered four AquaSnap® 30RB 402 air-cooled chillers to the historic Stormont site in Belfast, Northern Ireland, where the steeply raked track was built on the steps of the Parliament building. Carrier team worked closely with ice rink specialist AST Eistechnik GmbH of Austria, who designed, supplied and commissioned the refrigeration piping system and was responsible for the preparation and maintenance of the ice track.

Carrier's experience of delivering high specification cooling and heating for outdoor leisure events ensured the tight timetable for set-up and decommissioning was achieved, and the project was a resounding success.

Background

Described as one of the world's fastest sports, the competitive ice cross downhill competition was one of four Red Bull Crashed Ice outings staged over the year. The AquaSnap® chillers, with a combined cooling capacity of 1.6MW, circulated a 40:60 mixture of glycol and water at -10°C through the AST Eistechnik "Skateway" system, a flexible carpet of tubes, running the length of the track.

Once the chillers were connected up and commissioned, water was sprayed onto the freezing surface, taking ten days to produce a high quality layer of ice 4.5in thick along the 430m long track. In addition to chillers, Carrier Rental Systems also supplied two 400kW boilers, to provide hot water at 45deg C to melt the ice track after the culmination of the three-day competition.

Simon Ward, Carrier Rental Systems national events manager said: "It was a tremendous event, and attracted huge local and international interest. It also provided a superb application of temporary cooling in a spectacular setting, not to mention the equally important application of temporary heating." He further explained: "Once frozen, the ice track has significant thermal inertia, and the decommissioning required boilers to be connected up. The energy flowing through the Skateway piping system ensured the ice was gone in just two days."

In addition to chillers and boilers, Carrier Rental Systems supplied external pumps, buffer tanks, flanges, adapters and 300m of flexible hosing for the project.


carrier-case-study-crashed-ice-event-ice-track
Carrier capabilities
  • Carrier chillers provide critical cooling throughout the high profile event.
  • Carrier Rental Systems logistical expertise and project planning skills meet tight timescale.
  • Carrier's offering across cooling and heating delivers all thermal requirements. 
  • Carrier Rental Systems experience of supporting outdoor ice rinks provide total assurance for contractor and end user.
Technologies
  • 4 x AquaSnap® 30RB 402 aircooled chillers with Greenspeed® intelligence
  • 2 x 400kW boilers
  • Ancillaries: external pumps, buffer tanks, flanges, adapters and 300m of flexible hosing
Challenges and Solutions

The project presented a number of specific challenges:

  • On site logistics presented a challenge, with limited space for chillers and related equipment. Carrier's expertise enabled it to deliver and position equipment accurately alongside and beneath the raised track, reducing pipework distances and conforming with the track design.
  • The project had a tight timetable for delivery and commissioning. Carrier's project management and logistical skills enabled the event to achieve these, meeting timescale and budget targets.
  • The cooling requirement for the outdoor track was quite high, due to the size of the ice surface and variability of ambient conditions. Carrier's expertise in refrigeration enabled the load to be accurately calculated and catered for with high performance and reliable chillers.