Skip to main content

Carrier AquaSnap® Heat Pump Delivers Reliable, Clean Comfort for Yew Tree Nursery

AXBRIDGE, United Kingdom -

A high performance Carrier air-to-water heat pump is delivering comfortable ambient conditions for children and staff at Yew Tree Nursery in Axbridge, Somerset. Carrier’s AquaSnap 61AF heat pump was selected to replace an oil-fired heating system that was proving unreliable and inefficient. The Carrier unit captures low-grade heat energy from the atmosphere and upgrades it to generate hot water for use in the nursery’s underfloor heating, radiators and domestic hot water supply. Carrier, a world leader in high-technology heating, air-conditioning and refrigeration solutions, is a part of Carrier, a leading global provider of innovative heating, ventilating and air conditioning (HVAC), refrigeration, fire, security and building automation technologies.

“We chose the Carrier system as it enables you to match the exact requirements of an application, rather than simply supplying a standard factory-specification product, as with some other manufacturers,” said Tom Mangnall, who led the project for contractor, Somerset Mechanical Ltd. “The other major attraction was the plug-and-play design of the AquaSnap monobloc. It was delivered fully assembled, tested and charged with refrigerant and only required power and water connections, which saved time on site and reduced installation costs.”

The unit, which has an A+ energy rating, includes a soft-start system for low power draw, and freeze protection to maintain operation when outdoor temperatures dip. Even in temperatures down to minus 20 degrees Celsius, the unit can provide domestic hot water at up to 55 degrees Celsius. In addition to providing clean, reliable, high performance heating, it freed up space at the nursery, as the bulky fuel-oil storage tanks required by the previous system are no longer needed.

“The AquaSnap 61AF heat pump is compact and very versatile, and ideal for heating and domestic hot water production,” said Russ Tyrrell, senior technical sales engineer, Carrier. “We believe it has huge potential for wider use in the UK, particularly in similar applications that currently rely on oil-based systems. It is an ideal solution for use in homes, apartment buildings, shops, offices, restaurants, hotels, warehouses.”

About Carrier
Founded by the inventor of modern air conditioning, Carrier is a world leader in high-technology heating, air-conditioning and refrigeration solutions. Carrier experts provide sustainable solutions, integrating energy-efficient products, building controls and energy services for residential, commercial, retail, transport and food service customers. Carrier’s HVAC business is a part of Carrier, a leading global provider of innovative HVAC, refrigeration, fire, security and building automation technologies. For more information, visit www.carrieraircon.co.uk or follow @Carrier on Twitter.

carrier-aquasnap-61AF-330x295
The Carrier AquaSnap 61AF 045 air-to-water monobloc heat pump just requires water and power connections.

yew-tree-nursery-400x300
The Carrier heat pump at Yew Tree Nursery supplies radiators, underfloor heating and domestic hot water.