Passer au contenu principal

Carrier Introduces Improved Performance® Series Fan Coils

INDIANAPOLIS, Ind. -

Carrier is pleased to announce the release of improved Performance Series fan coils that will facilitate easier installation with a nearly 20 percent smaller footprint. Carrier, the world’s leader in high-technology heating, air-conditioning and refrigeration solutions, is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp. (NYSE: UTX).

The enhanced Performance Series fan coil will offer factory-installed electric heat options as well as increased flexibility for single-stage demand dehumidification. The new units will be available in two options: a 2-ton 15 seasonal energy efficiency rating (SEER) with a 14-inch wide cabinet and a 5-ton 15 SEER rating with a 21-inch wide cabinet. Impressive 15 SEER ratings are achieved in smaller spaces than previously available Performance Series fan coil systems.

“Carrier understands the unique challenges heating and cooling technicians face when working in tight spaces to install or service a system. We designed this enhanced set of Performance Series fan coils knowing that every single inch we take off the unit can simplify installation for technicians in the field,” said Matthew Pine, vice president, marketing, Carrier Residential. “Moreover, the unit’s enhanced dehumidification illustrates our commitment to total home comfort.”

The improved fan coils are compatible with single- and two-stage outdoor units and deliver two-stage blower operation. These fan coils achieve a wider airflow range and include a lower continuous fan option than FB4C and FX4D fan coils, resulting in lower electric bills and lower sound levels.

About Carrier
Carrier is the world’s leader in high-technology heating, air-conditioning and refrigeration solutions. Carrier experts provide sustainable solutions, integrating energy-efficient products, building controls and energy services for residential, commercial, retail, transport and food service customers. Founded by the inventor of modern air conditioning, Carrier improves the world around us through engineered innovation and environmental stewardship. Carrier is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. Visit www.carrier.com for more information or follow the company on Twitter: @CarrierGreen.


Carrier Performance™ Series Fan Coil