Skip to main content

Carrier Transicold Launches X4 7300 Trailer Refrigeration Unit in India

MUMBAI, India -

New single-temperature unit delivers advanced cooling performance and precise temperature control in ambient conditions up to 50°C

Carrier Transicold today launched the X4™ 7300 single-temperature trailer refrigeration unit in India, where it is now commercially available, expanding its portfolio for fleets transporting temperature-sensitive food, pharmaceuticals and other perishable cargo. Carrier Transicold is part of Carrier Global Corporation (NYSE: CARR), global leader in intelligent climate and energy solutions.

Designed for demanding temperature-controlled transport applications, the X4 7300 combines strong refrigeration performance with precise temperature control and an efficient operating platform to help fleet operators maintain the conditions required to protect temperature-sensitive cargo across increasingly complex distribution routes.

“As India strengthens the infrastructure connecting producers, distribution centers and end markets, fleets need refrigeration equipment that can protect temperature-sensitive cargo efficiently across longer and more demanding routes,” said Pankaj Mehta, Managing Director, Truck Trailer India, Carrier Transicold. “We see trailer refrigeration emerging as an important new category for temperature-controlled transportation. The X4 7300 is designed to help operators meet these evolving demands while managing operating costs, and it underscores our commitment to supporting the continued development of India’s cold chain with advanced, efficient refrigeration solutions.”

Engineered with EcoFORWARD™ technologies, the X4 7300 delivers dependable refrigeration performance in ambient temperatures of up to 50°C, making it well suited to the demanding conditions of India's temperature-controlled distribution network. Reduced engine run hours and lower maintenance costs compared to legacy units can also help lower the total cost of ownership for fleet operators.

The X4 7300 features Carrier Transicold’s APX™ Control System, which coordinates refrigeration components to help optimize performance and fuel efficiency while supporting precise temperature control, system reliability and ease of operation.

For more information about Carrier Transicold India products and services, visit www.carriertransicoldindia.com. 

About Carrier Transicold

Carrier Transicold helps improve transport and shipping of temperature-controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 50 years, Carrier Transicold has been an industry leader, providing customers around the world with advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of Carrier Global Corporation, global leader in intelligent climate and energy solutions that matter for people and our planet for generations to come. For more information, please visit us at Carrier.com/truck-trailer/en/in or follow us on LinkedIn at Carrier Transicold Truck Trailer Refrigeration.

Carrier Transicold Launches X4 7300 Trailer Refrigeration Unit in India