Carrier Transicold Launches Vector 8200 Engineless TRU for On-site Cold Storage
ATHENS, Ga. -
Carrier Transicold has introduced the Vector™ 8200, an all-electric, engineless refrigeration unit with single and multi-temperature capabilities designed for trailers used as stationary cold storage. Carrier Transicold is part of Carrier Global Corporation (NYSE: CARR), global leader in intelligent climate and energy solutions.
The Vector 8200 uses electricity from the grid or other external power sources, eliminating the fuel consumption, emissions, noise and operating costs associated with a diesel-powered engine and generator. Its TRU-Demand E-Drive™ energy management system monitors the power draw and adjusts to changes in a facility’s electrical supply, maintaining voltage during brownout conditions and preventing grid strain when multiple units restart after power outages. Four remote evaporator choices provide flexibility to cool one-, two- or three-compartment trailers.
“As companies seek to manage their operating costs and impact on neighbors and the environment, the Vector 8200 is a quiet, durable, intelligent all-electric solution for single- or multi-temperature trailer storage,” said Arthur Pluta, Electrification Product Manager, Truck Trailer Americas, Carrier Transicold.
Other benefits of the Vector 8200 include:
- Exceptional cooling capacity: The Vector 8200 delivers up to 58,000 BTU/hr at 35°F, ensuring reliable temperature control for sensitive cargo. It also provides electric heating and defrost.
- Advanced APX™ controls: Features IntelliSet™ technology with ProductShield™ for precise temperature management.
- Lynx Fleet™ telematics integration: Provides comprehensive fleet intelligence, monitoring and two-way control capabilities.
- Engineered for reliability: The Vector 8200 features a fully hermetic electric scroll compressor, high-efficiency microchannel condenser, maintenance-free AC fan motors and an electronic expansion valve. Options include a high-power 40-amp battery charger and a TRU-mounted solar charging system.
For more information about the Vector 8200 and Carrier Transicold’s complete range of transport refrigeration solutions, visit the Carrier Transicold booth, number 6767, at the Advanced Clean Transportation (ACT) Expo from April 28 to May 1 in Anaheim, California, or contact the experts in Carrier Transicold’s North American dealer network.
* The Vector 8200 is an engineless trailer option that creates no direct emissions. However, indirect emissions and refrigerant leaks are possible.
About Carrier Transicold
Carrier Transicold helps improve transport and shipping of temperature-controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 50 years, Carrier Transicold has been an industry leader, providing customers around the world with advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of Carrier Global Corporation, global leader in intelligent climate and energy solutions that matter for people and our planet for generations to come. For more information, visit Carrier Transicold at www.trucktrailer.carrier.com. Follow Carrier on X at @SmartColdChain, on Facebook at Carrier Transicold Truck/Trailer Americas and on LinkedIn at Carrier Transicold Truck Trailer Refrigeration.