Carrier Transicold Adds TRU Battery Protection to BluEdge Service
Ga, ATHENS -
Carrier Transicold’s BluEdge™ service platform now offers fleets protection from expenses related to premature failure of transport refrigeration unit (TRU) batteries, provided that the TRU is supported by a Carrier Transicold solar charging system. Carrier Transicold is part of Carrier Global Corporation (NYSE: CARR), global leader in intelligent climate and energy solutions.
“This industry-leading coverage for refrigerated trailers can significantly reduce the risk of premature battery failure while also assuring the battery will be quickly replaced – hassle free, parts and labor included – by Carrier Transicold’s extensive dealer network throughout the U.S. and Canada if it fails to start the TRU within the contract coverage,” said Stuart Johnson, BluEdge Commercial Lead, Carrier Transicold.
During extended dwell periods, even fresh TRU batteries can be drained by current draw from peripheral devices, including telematics systems that are now widely used by fleets.
“Our TRU Battery Protection option helps avoid a leading reason for emergency call-out service, premature battery failure because an out-of-service TRU simply ran out of fuel and couldn’t charge the battery via its alternator,” Johnson said. “Solar panels maintain battery charge without requiring the TRU to run, saving fuel, ensuring uninterrupted performance and helping fleets avoid these inconvenient and potentially costly situations.”
TRU Battery Protection requires a Carrier Transicold unit to have:
- A BluEdge Core or Elite service plan.
- A PowerRush™ wet cell or PowerRush Platinum (AGM) battery, both of which are engineered to meet tough cycling demands of TRU applications.
- A Carrier Transicold solar charging system.
The TRU Battery Protection option also extends the standard warranty of PowerRush wet cells from 18 months to two years.
Carrier Transicold’s TRU Battery Protection applies to X4™ 7000 and Vector™ 8000 series trailer units, Vector HE 19 and 1550 intermodal systems, and the Solara heating unit. Coverage can be applied to existing TRUs already equipped with Carrier Transicold solar charging systems and PowerRush batteries.
For more information about TRU Battery Protection, turn to the experts in Carrier Transicold’s North America dealer network.
About Carrier TransicoldCarrier Transicold helps improve transport and shipping of temperature-controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 50 years, Carrier Transicold has been an industry leader, providing customers around the world with advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of Carrier Global Corporation, global leader in intelligent climate and energy solutions that matter for people and our planet for generations to come. For more information, visit www.trucktrailer.carrier.com. Follow Carrier on Twitter: @SmartColdChain, on Facebook at Carrier Transicold Truck/Trailer Americas and on LinkedIn at Carrier Transicold Truck Trailer Refrigeration.