Evaporator Coils vs. Condenser Coils
The main difference between an evaporator coil and a condenser coil is their location and purpose within your HVAC system. The evaporator coil is located inside your home and absorbs heat, while the condenser coil is located outside and releases that heat into the environment.
Have you been asking yourself how these two vital components differ? The world of advanced HVAC systems can be complex, and understanding the distinctions between these two crucial components is essential for maintaining long-term comfort and energy efficiency. In this article, we will dive into the intricate workings of evaporator coils vs. condenser coils so you can make confident, informed decisions about your home climate.
What Is A Coil In An Air Conditioner?
In an air conditioning system, a coil is a critical heat transfer component that actively cools your home by moving heat from one place to another.
Air conditioning systems typically feature two types of coils: the evaporator coil and the condensing coil. These coils are typically crafted from high-quality copper or aluminum. These materials offer excellent heat transfer properties and long-lasting durability, making them highly reliable for a coil’s demanding function. By leveraging advanced materials, modern coils help ensure your system operates efficiently, ultimately helping to reduce your energy bills.
What Is An AC Evaporator Coil?
An AC evaporator coil is located inside the indoor unit of an air conditioning system and is responsible for absorbing the heat from your indoor air.
This coil contains a network of tubes—often made of copper or aluminum—that facilitate the cooling process. As the liquid refrigerant passes through the indoor coil, it undergoes a phase change into a gas. This transformative process absorbs heat from the surrounding air, thereby cooling it down. The cooled, comfortable air is then seamlessly circulated back into your living spaces, improving your overall indoor environment.
Clint Newsome, owner of Albany Air Conditioning and Heating Co. in Albany, GA explains that the evaporator coil plays a critical role in how a split HVAC system cools and dehumidifies a home.
“Your evaporator coil on a split system is located on your indoor unit—the unit you see inside the home if you have a split system,” Newsome said. ‘It’s where warm indoor air is pulled across a network of cold refrigerant-filled coils. As the air passes over the coil, the refrigerant absorbs heat from the air, cooling it down before it is circulated back through your home. At the same time, moisture in the air condenses on the coil, helping reduce humidity levels and improving indoor comfort.”
Learn more about what is an evaporator coil.
What Is A Condenser Coil?
A condenser coil is located in the outdoor unit of an air conditioning system and is responsible for releasing the heat that was absorbed from inside your home.
Much like its indoor counterpart, the condenser coil consists of a robust network of tubes. When the refrigerant, now in a hot gaseous state, flows through the outdoor condenser coil, it releases the absorbed heat into the outside environment. This vital heat transfer process causes the refrigerant to condense back into a liquid form. The condensed refrigerant is then pumped back inside to the evaporator coil to repeat the efficient cooling cycle.
“The condenser coil is the component wrapped around the outdoor unit,” Newsome said. “As air moves through the system, it passes across the coil, where heat is transferred before the air is discharged through the top of the unit.”
How Do AC Evaporator Coils and Condenser Coils Work Together?
Evaporator and condenser coils work together in a continuous, seamless cycle to remove heat from your home and expel it outside.
Refrigerant enters the evaporator coil through copper tubing connected to your outdoor unit. Once inside, it absorbs the heat from the air blowing over it. Simultaneously, moisture in the air is condensed into water on the coils, which then reliably empties into the drain pan. Removing this excess moisture lowers the temperature of the air blown into your home, creating a more comfortable and breathable environment.
The now-warm refrigerant flows to the outdoor unit. It then runs through the condenser coil, where the heat is quietly and efficiently expelled to the outdoor air. Finally, the liquid refrigerant travels back inside to the evaporator coil to repeat the process, delivering the reliable performance homeowners expect.
Newsome added that keeping both coils clean is important for efficiency and system longevity.
“It's important to keep the condenser coil clean, which homeowners can do with a typical water hose spraying it off,” Newsome said. “I wouldn't put a sprayer on the end of your hose, but I would just use your hose just to wash it off and get the dirt and debris off of it."
Learn More About Air Conditioner Evaporator Coils and Condenser Coils
Schedule an appointment with your local Carrier dealer to get all of your evaporator coil and condenser coil questions answered, and to get a state-of-the-art Carrier HVAC system installed at your home. Carrier dealers provide standout installation, maintenance, and service of condenser coils, evaporator coils, and all advanced HVAC products.
Frequently Asked Questions
It is not recommended to use evaporator coil cleaner on condenser coils unless the cleaner is specifically labeled for both. Evaporator coil cleaners are often designed for indoor use and may not be strong enough to handle the dirt, grease, and debris that accumulate on outdoor condenser coils. Using the wrong cleaner could reduce effectiveness or damage the coils.
AC evaporator coils are located inside the home, typically within or near the indoor fan coil or furnace.
It is highly recommended to replace the evaporator coil when replacing the condenser. Mismatched coils can lead to efficiency issues, reduced system performance, and increased wear on the new condenser. To ensure proper compatibility and energy efficiency, both components should ideally be replaced together, especially if the system is older.
No, evaporator and condenser coils are not the same. The evaporator coil is located inside the home and absorbs heat from indoor air, while the condenser coil is located outside the home and releases that heat by condensing the refrigerant back into a liquid.
Dirty evaporator or condenser coils restrict airflow and insulate the coils, reducing heat transfer efficiency. This forces your HVAC system to work harder and run longer, which significantly increases energy consumption and can lead to higher monthly energy bills.
Common indicators that your coils need attention include reduced cooling capacity, unusually high energy bills, the system running constantly, or ice forming on the indoor evaporator coil. Learn more about AC maintenance.
About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.