The versatile new Vector™ 8611MT, a multi-temperature trailer refrigeration unit, enables a trailer to be divided lengthwise into two refrigerated compartments. Introduced today by Carrier Transicold at the Distribution Solutions Conference of the International Foodservice Distributors Association, the Vector 8611MT unit incorporates two evaporators and fans for two-zone cooling without requiring a separate remote evaporator. Carrier Transicold is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp. (NYSE: UTX).
“The Vector 8611MT unit harnesses the innovative Vector platform to create a highly efficient, high-performance unit for center-divide trailers where the perishable and frozen compartments are side by side,” said Patrick McDonald, product manager, trailer products, Carrier Transicold. “The all-electric architecture of the Vector series enables the unit to independently manage the two zones more simply and efficiently than mechanically interconnected competitive units.”
“The Vector 8611MT unit will especially appeal to food service and grocery distribution operations for the flexibility it offers in creating center-divide configurations,” McDonald added. “Uniquely, our split evaporator design creates a 15-inch-wide area for center-wall placement, providing a more efficient accommodation of pallets that allows up to 17 percent more cargo than competitive systems requiring trailers to be divided precisely down the middle.”
As with other units in Carrier Transicold’s Vector platform, the new unit features E-Drive™ all-electric technology, in which the diesel engine runs a 21 kVA electric generator that powers the refrigeration system. Vector units have built-in electric standby capability, so when parked for loading, unloading or staging, they can be operated via an electric power source, providing full refrigeration capacity while eliminating refrigeration unit engine noise, emissions and fuel consumption.
The innovative Vector 8611MT unit architecture eliminates most refrigerant valves and significantly reduces the number of braze joints and potential refrigerant leak points compared to mechanically interconnected competitive models. Uniquely, the Vector 8611MT unit has independent air control, enabling it to optimize airflow and pulldown to both zones. If heating is required, it has the advantage of consistent electric heat, rather than hot gas heat. This reduces system complexity and enables the unit to shut down the compressor and other refrigeration components when heating is required, greatly reducing the power load on the engine, resulting in further fuel savings.
The Vector platform’s reduced system complexity also simplifies diagnostics and maintenance requirements for service technicians.
For additional details on the Vector 8611MT trailer refrigeration unit, which will be commercially available in the first quarter of 2019, turn to the experts in Carrier Transicold’s North America dealer network.
About Carrier Transicold
Carrier Transicold helps improve transport and shipping of temperature-controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 45 years, Carrier Transicold has been an industry leader, providing customers around the world with advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. For more information, visit www.transicold.carrier.com. Follow Carrier on Twitter: @SmartColdChain.