Bute-based haulier, John Mackirdy Limited, has taken delivery of a new Carrier Transicold Vector® HE 19 MT (multi-temperature) refrigeration unit, mounted to the company’s first ever double-deck trailer. The new asset is designed to increase fleet efficiency and improve sustainability across the business. Carrier Transicold is a part of Carrier Global Corporation (NYSE: CARR), a leading global provider of innovative heating, ventilating and air conditioning (HVAC), refrigeration, fire, security and building automation technologies.
The new 13.6-metre double deck – manufactured by Gray & Adams – joins John Mackirdy Limited’s 10-strong mixed commercial vehicle fleet, which includes two standard refrigerated trailers mounted with Vector 1950 MT units and one 12-tonne rigid with a Carrier Transicold Supra® 450 unit.
“All of our refrigerated vehicles are Carrier-cooled; when it comes to new trailers we always specify the latest Vector, and they’ve never let us down,” said John Mackirdy, managing director, John Mackirdy Limited. “As a business, we’re now looking at ways to reduce our carbon footprint and future proof our fleet; the new double deck will play a major role in this. We’ll be able to combine substantial fuel savings from the Vector with almost double the load space, meaning we make far fewer journeys.”
The new Vector HE 19 MT combines Carrier Transicold’s all-electric E-Drive™ technology with a new ultra-modern multi-speed engine design that can cut fuel consumption by up to 30%. The unit also offers a 10% savings in weight and a noise reduction of 3 dB(A) – which to the human ear equates to 50% less noise. The system also delivers up to 15% savings on maintenance costs.
The fully hermetic scroll compressor and economiser helps increase refrigeration capacity during pull-down by 40%, while cutting the chance of refrigerant escape by 50%. When plugged into the electrical grid on standby, the Vector HE 19 MT is also 19% more efficient, meaning it delivers reduced diesel, maintenance and electricity bills.
“The list of benefits we get from the new Vector HE 19 MT are fantastic. Not only do they help us deliver on the environmental front, but they also drive down operating and running costs – which in the current climate is extremely important,” said Mackirdy.
John Mackirdy Limited has also opted for Carrier Transicold’s advanced telematics package for the first time. Using two-way communication, the system offers the ability to remotely alter set points or operation modes, as well as initiate defrosts, pre-trip checks, and clear alarms from any connected device. The new Vector HE 19 MT also features Carrier Transicold’s DataCOLD™ 600 temperature recorder, which provides easy access to a wealth of information on unit performance.
The new unit is also covered by everCOLD™, Carrier Transicold’s fixed cost, full-service maintenance package that includes annual temperature control testing and certification, full regulatory checks and access to Carrier Transicold’s oneCALL™ 24/7 incident management service.
Expected to stay in operation for 10 years, the new trailer will transport goods for a variety of customers. However, it will primarily be used for the distribution of food products from a local producer into mainland Scotland.
For more information on Carrier Transicold and its products and services, visit carriertransicold.co.uk. Follow Carrier Transicold on Twitter @SmartColdChain and on LinkedIn at Carrier Transicold Truck Trailer Refrigeration.
About Carrier Transicold
Carrier Transicold helps improve transport and shipping of temperature controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 50 years, Carrier Transicold has been an industry leader, providing customers around the world with advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of Carrier Global Corporation, a leading global provider of innovative HVAC, refrigeration, fire, security and building automation technologies. For more information, visit carriertransicold.co.uk. Follow Carrier on Twitter: @SmartColdChain and on LinkedIn at Carrier Transicold Truck Trailer Refrigeration.
John Mackirdy has taken delivery of a new Carrier Transicold Vector® HE 19 MT (multi-temperature) refrigeration unit, mounted to the company’s first ever double-deck trailer.