Carrier Transicold is offering a provision to use R-513A refrigerant with its PrimeLINE® container unit for customers seeking a refrigerant with lower global warming potential (GWP), or as a hedge against potential regulatory changes that may affect the availability and prices of traditional hydrofluorocarbon (HFC) refrigerants. Carrier Transicold is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp. (NYSE: UTX).
“Phasedowns of traditional HFC refrigerants due to their higher GWP have raised concerns about their future availability and pricing, and some of our customers have indicated an interest in using R-513A as an alternative,” said Willy Yeo, director of marketing, global container refrigeration, Carrier Transicold.
R-513A, a new synthetic blend of the hydrofluoroolefin R-1234yf and R-134a, has a GWP of 631, which is significantly lower than those of HFC refrigerants conventionally used in container refrigeration systems.
For customers acquiring new PrimeLINE refrigeration units, Carrier Transicold is providing a “513A-ready” provision. It features a new digital scroll compressor designed for use with R-513A, as well as traditional R-134a. The units will be sold with R-134a, enabling customers to switch to R-513A at a time of their own choosing. Conversions require a simple kit that includes a software update and replacement filter dryer.
“Fleets that want to use a more sustainable refrigerant and also want to hedge against price and availability issues associated with synthetic refrigerants should first consider Carrier Transicold’s natural-refrigerant NaturaLINE® unit,” Yeo said. “The NaturaLINE unit offers efficiency, quiet operation, tight temperature control, a deep frozen capability that goes to -40 degrees Celsius, and uses carbon dioxide, an ultra-low GWP refrigerant.”
The NaturaLINE unit’s combination of efficiency and use of an ultra-low GWP refrigerant reduces carbon emissions by 28 percent compared to earlier models.
With a GWP of 1, CO2 refrigerant takes refrigerated container customers to an end-state, bypassing the need for intermediate solutions such as R-513A, which will be subject to phase outs within the 15-year lifespan of units purchased today.
Availability of the 513A-ready PrimeLINE unit is anticipated in the first quarter of this year. Conversion kits will be available beginning later in the year. For more information about refrigerant options for container shipping from Carrier Transicold, visit www.carrier.com/container.
About Carrier Transicold
Carrier Transicold commemorates its heritage of container refrigeration innovation and leadership in 2018 by marking the 50th anniversary of its pioneering front-wall container refrigeration unit design. Carrier Transicold helps improve transport and shipping of temperature-controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. Carrier Transicold is an industry leader, providing customers around the world with advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. For more information, visit www.transicold.carrier.com. Follow Carrier on Twitter: @SmartColdChain.