Carrier Transicold Strengthens Sustainability Initiatives with Lower GWP Refrigerant for North America Truck and Trailer Systems

ATHENS, Ga. -

As a leader in providing environmentally sustainable transport refrigeration solutions, Carrier Transicold has begun offering North America’s refrigerated haulers the new-generation refrigerant R-452A as an option for new and existing equipment. Carrier Transicold is a part of Carrier Global Corporation (NYSE: CARR), a leading global provider of healthy, safe and sustainable building and cold chain solutions.

Starting in the first quarter of 2021, purchasers can specify R-452A on all Carrier Transicold trailer and diesel truck equipment orders. Carrier units with R-452A refrigerant have performance comparable to Carrier units with R-404A, the traditional transport refrigerant, in terms of refrigerant capacity, pulldown, fuel efficiency and reliability.

“R-452A has a global warming potential (GWP) of 2140, which is about half that of R-404A (GWP 3922),” said Bill Maddox, senior manager, product management, Carrier Transicold. “We are offering it for fleets that want to improve their environmental profiles and to prepare for compliance with evolving regulations.”

The California Air Resource Board (CARB) has proposed prohibiting high GWP refrigerants on new transport refrigeration equipment starting in 2022. Additionally, Canada has banned high GWP refrigerants for new transport refrigeration starting in 2025, in keeping with its plans to reduce greenhouse gas emissions in accordance with the Kigali Agreement of the Montreal Protocol. In the U.S., the Environmental Protection Agency has approved the use of R-452A for transport applications but has not prohibited continued use of R-404A.

While there are currently no retrofit regulations proposed, Carrier Transicold units already in service can easily take advantage of R-452A. For Carrier units with an electronic expansion valve, converting requires only an operating software update. On Carrier Transicold truck units and older trailer units that use a mechanical expansion valve, the valve will require a manual adjustment or replacement, depending on the model.

Refrigerant cost may be a factor for some fleets considering conversion to R‑452A, Maddox said. Currently R-452A is three to four times more expensive than R‑404A, which will add somewhat to the initial equipment purchase and could affect refrigerant-related repair costs.

“Still, haulers should start to consider when transitioning to a lower GWP refrigerant will make the most sense for their fleets,” Maddox said. “While the EPA permits continued use of R-404A, the proposed 2022 California changes may ultimately drive use of R-452A as a de facto national standard, due to the large volume of refrigerated traffic that moves into that state.”

For more information about R-452A for transport refrigeration applications, turn to the experts within Carrier Transicold’s North America dealer network.

TTA-127-Carrier-Transicold-offers-lower-GWP Refrigerant-for TRUs_12152020
Carrier Transicold in North America has begun offering R-452A, a refrigerant option with nearly half the global warming potential (GWP) of the traditional truck and trailer refrigerant. Offering a lower GWP refrigerant for transport solutions is one way Carrier supports the safe, sustainable transport of perishables through the cold chain.

About Carrier Transicold
Carrier Transicold helps improve transport and shipping of temperature-controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For 50 years, Carrier Transicold has been an industry leader, providing customers around the world with advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of Carrier Global Corporation, a leading global provider of healthy, safe and sustainable building and cold chain solutions. For more information, visit transicold.carrier.com. Follow Carrier on Twitter: @SmartColdChain, on Facebook at Carrier Transicold Truck/Trailer U.S. & Canada and on LinkedIn at Carrier Transicold Truck Trailer Refrigeration.