Routine Issues that Could Affect the Performance of Your Chillers

11/01/2016 08:00:00


Chillers are used in a wide variety of capacities. Common applications for air-cooled and water-cooled chillers include food processing plants, ice rinks, hospitals, cold storage and warehousing, chemical and refinery production projects, and process cooling. Chillers are incredibly important for comfort cooling, emergency response, and other situations as well. This is why it’s extremely important that they are maintained to perform at peak performance.

In addition to that, chillers can easily represent a significant portion of a building’s utility bill for the month if proper care isn’t maintained. Moreover, many service calls can be avoided altogether with simple maintenance. Given their importance, you might be wondering then how to ensure your facility’s chillers remain in tip top shape. Here are several things to keep in mind:

Today’s Modern Chillers Feature Advanced Diagnostics with Alarm Codes: All you might need is your owner’s manual to determine what the problem is. When there is an issue, many chillers will display a code that corresponds to the issue. This could help you determine what the best course of action is to fix it. Do not ignore a code as this will only worsen the problem and potentially cause further issues with the chiller.

Don’t Try to Use the Chiller for an Application It Isn’t Suited for: Every chiller has its own limit in regard to what it can handle and what it can’t. For example, overloading it with too much water or air to increase its capabilities will only cause the chiller to become less efficient. This is why it’s extremely important to purchase chillers that match your needs and facility’s capabilities.

Don’t Overlook Corrosion: Corrosion is an unfortunate commonality with chillers. It is caused by sediment build-up and it can eventually lead to the chiller no longer working. This is why regular maintenance is crucial to the long-term productivity of the chiller. In addition to checking for corrosion, be sure to keep a maintenance schedule to make routine updates and check for minor issues before they become major problems. Chillers can quickly downgrade when the care isn’t put in.

What Do You Do If You Need a Major Repair or Replacement?


These are just several of the things you can do to ensure a long life for your chillers. If you do find that you are having an issue with your chillers, you might have to have them serviced or replaced. Our team at Carrier Rental Systems can help you mend the gap in services by providing stellar, best-in-class chiller rentals that meet the requirements of your project or operations.

We have air-cooled and water-cooled chillers to choose from, and we have chillers in many different sizes to meet your needs. Remember, one of the biggest issues concerning chillers is size. Choosing the wrong size can affect performance and energy efficiency. We will make sure this doesn’t happen. We have installed chillers for a wide variety of applications, and we can design a customized solution that includes quick project turnaround. Contact us today if you run into an issue with your chillers and need chiller rentals to maintain operations.

Carrier Transicold, Truck/Trailer, Europe Media Contact Aline Lucas Send An Inquiry