Healthcare Hospital Boiler Hire - 100kW Boiler Hire -
London
London’s Kings’ College Hospital required a temporary heating solution during planned maintenance work on its boiler, in a project lasting eight weeks..
What Did We Do?
Carrier Rental Systems provided a temporary hire boiler to enable the hospital to continue operating, while the contractor carried out the refurbishment work on the existing boiler over a two-month period.
How Did We Do It?
The CRS regional sales manager for London carried out a full site survey, and advised the customer on what size boiler would be required, how the hire system would be connected to the existing system, and identified a suitable location at the rear of the building to position the hire boiler.
Equipment – CRS 100 Boiler, CRS Fuel Tank, Pipe Work, Fittings & Cable
End User – Kings College Hospital, London
Application – Heating, LTHW
Additional – Single Phase 240v Boiler
Healthcare
Low Temperature
Hot Water /
Heating Hire
London
100kW Boiler Hire

The customer was highly satisfied with the hire solution, which allowed refurbishment work on the existing boiler to proceed while the hospital continued to operate and deliver normal services to patients without interruption.
Commenting on the project, the CRS Sales Director said: “We have recently invested in our boiler hire fleet due to increased demand from contractors and end users, such as hospitals, hotels, courts, and manufacturing plant sites. Our latest range of boilers includes models that operate on a 240V supply, including our 400kW hire boiler.”
| APPARATUUR | 2 x CH0149 |
| EINDGEBRUIKER | Datacenter |
| TOEPASSING | Tijdelijke koeling van een datacenter |
| ADDITIONEEL | Buffervat, warmtewisselaar, kabels en leidingen |