Carrier helps a central London hotel upgrade its HVAC
system quickly and seamlessly with an airlift delivery of
two new AquaSnap® chillers
Customer – Hilton Metropole Hotel
Location – London, UK
Equipment Running Since – December 2014
Project
Carrier co-ordinated delivery of two new chillers to the Hilton Metropole Hotel with the help of a specialist lift helicopter, ensuring the replacement chillers were installed and operational quickly. Following a detailed health and safety assessment, which required co-ordination of aviation approvals for flights over central London, the company managed the decommissioning and removal of the two existing chillers from the building’s rooftop, and their replacement by the new Carrier AquaSnap® chillers. The entire operation was safely completed in less than fifteen minutes.

Hotel
Chiller
Replacement
London
522kW Chiller Hire

The original plan was to use a heavy-duty crane to remove two existing R22 refrigerant-based chillers from the rooftop of the Hilton Metropole Hotel and replace them with two new high-efficiency Carrier AquaSnap units, delivering a combined cooling capacity of just over 1MW.
However, concerns arose over the crane’s size and the load-bearing capacity of the road beneath, which passes directly over London Underground’s Central Line. The initial proposal would have required a long-term closure of Edgware Road—a major arterial route into central London—causing significant logistical challenges and disruption to the local community.
With the final phase-out of R22 refrigerant looming under EU legislation, Carrier devised an innovative solution by contracting Helirig and their Swiss helicopter partners to conduct the rooftop lift. A comprehensive risk assessment was undertaken, with all identified risks either mitigated or managed appropriately. Carrier also secured the necessary airspace permissions, and the helicopter lift proceeded as planned.
Les Cordery, Facilities Manager at the Hilton Metropole Hotel, said: “I am delighted at the speed and professionalism with which Carrier carried out the installation, and with no disruption to traffic or disturbance to our surrounding residents. We had been prepared for the project to take many months, since closing part of the busy Edgware Road to traffic isn’t an easy thing to arrange. However, Carrier’s innovative thinking and project management expertise provided an ideal solution and an unexpectedly timely result for the hotel.”
Carrier continues to support the installation, providing ongoing service and maintenance for the chillers to ensure optimum guest comfort, operational efficiency, and minimal running costs for the hotel.
Key Advantages
- Fast and safe removal of existing chillers from building roof and delivery of new chillers
- HVAC plant downtime minimised, ensuring service was maintained to hotel guests and revenue protected
- No requirement to apply for road closures and project site permits for heavy-duty cranes
- No disruption to traffic or the neighbourhood linked to delivery and installation
Technologies
- 2 x Carrier 30RB 522 AquaSnap® Air-Cooled liquid Chillers
Challenges and Solutions
The project presented several specific challenges, and the resulting solution succeeded in:
- Seamless installation: no disruption of service to the hotel;
- Innovative, safe and fast delivery via air: no delays due to road closure permit request process;
- Optimal security: no safety concerns about the load bearing capability of surrounding roads.