Skip to main content

D Steven & Son Equips New Trailer with Vector HE 19 MT Unit for Sustainability and Low Noise Emissions

WARRINGTON, England -

The most northerly haulage company on the UK mainland is celebrating its centenary with the delivery of a new Gray & Adams trailer mounted with Carrier Transicold’s flagship Vector HE 19 MT (multi-temperature) refrigeration unit. Carrier Transicold is a part of Carrier Global Corporation (NYSE:CARR) a leading global provider of healthy, safe and sustainable building and cold chain solutions.

Scrabster-based D Steven & Son, which also has depots in Aberdeen, Glasgow and Wick, has a long history of specifying Gray & Adams trailers with Carrier Transicold refrigeration units.

The latest delivery, part of an order for six trailers, stands out for being the first in the fleet to benefit from the latest generation Vector HE 19 MT unit – which improves fleet efficiency and sustainability. To mark the anniversary, the trailer’s rear barn doors carry the message ‘Servicing Caithness for over 100 years’.

“Being based in one of the most remote parts of Scotland means we need to have absolute confidence in the trucks and trailers we buy for the fleet,” said David Steven, managing director, D Steven & Son. “The Gray & Adams and Carrier Transicold combination works extremely well; we operate all the way down to mainland Europe and we enjoy superb reliability. There’s simply no need to look elsewhere.”

The new 13.6m single-deck trailer joins a fleet of 30 trucks and 50 trailers and will remain in service for the next five years, operating up to seven days per week.

“This is our first Vector HE 19 MT, and it should help us to achieve major performance advantages in almost every area – including a considerable improvement in fuel efficiency,” said David Steven Jr, director, D Steven & Son. “Plus, it’s around 50% quieter than the Vector 1950 we’ve been buying for years, so it’ll be particularly popular with our drivers.”

The Vector HE 19 also benefits from a fully hermetic scroll compressor and economiser which help to deliver a significant increase in refrigeration capacity during pull-down, while reducing the chance of refrigerant and carbon dioxide (CO2) escape, making it an environmentally sustainable choice. Customers can enjoy favourable savings on maintenance costs, thanks to a combination of the new features and extended service cycles. Carrier provides sustainable, effective refrigerated transport solutions for customers, part of its Healthy, Safe, Sustainable Cold Chain Program.

The trailer features high-gloss impact resistant five-element panels and is mounted on a heavy-duty twin member chassis, designed to withstand the demands of long-distance international haulage. Other features include a step neck chassis to reduce overall height, fuel saving vortex generator at the rear of the roof, fully waterproof aluminium floor surface and Michelin tyres as original equipment.

D Steven & Son operates a high-profile fleet, and due to the company’s remote location it is very flexible in the work it carries out, handling all transport requirements – including supporting the gas, supermarket and general haulage markets. Its trucks typically clock up around 100,000 miles per annum, with all routine refrigeration unit maintenance taken care of by Carrier Transicold South & Central Scotland.

For more information on Carrier Transicold and its products and services, visit www.carriertransicold.co.uk. Follow Carrier Transicold on Twitter: @SmartColdChain or on LinkedIn at Carrier Transicold Truck Trailer Refrigeration

About Carrier Transicold
Carrier Transicold helps improve transport and shipping of temperature-controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 50 years, Carrier Transicold has been an industry leader, providing customers around the world with advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of Carrier Global Corporation, a leading global provider of healthy, safe and sustainable building and cold chain solutions. For more information, visit www.carriertransicold.co.uk.  Follow Carrier on Twitter: @SmartColdChain and on LinkedIn at Carrier Transicold Truck Trailer Refrigeration.

D Steven & Son G&A trailer with Vector HE 19 MT refrigeration unit
D Steven & Son, the most northerly haulage company on the UK mainland, is celebrating its centenary with the delivery of a new G&A trailer mounted with our flagship Vector HE 19 MT refrigeration unit.