Skip to main content

Carrier Introduces Infinity Return Air Purifier to Help Inactivate Coronavirus in Filtered Air

INDIANAPOLIS -

As part of a strategy for improving indoor air quality in the home, the return air purifier should be considered essential

Today’s tightly constructed, energy-efficient homes have one disadvantage – it can be difficult for airborne pollutants to escape. In order to address this, Carrier recently launched the Infinity® return air purifier, its latest indoor air quality solution designed to help create a healthier home. Installed and mounted in the return air duct, the air purifier offers proven, third-party tested effectiveness in inactivating 99% of select airborne viruses and germs, including coronavirus1 trapped by the MERV 15 filter. Carrier is a part of Carrier Global Corporation (NYSE: CARR), a leading global provider of healthy, safe, sustainable and intelligent building and cold chain solutions.

The Infinity return air purifier, a part of the Healthy Homes suite of Carrier’s Healthy Buildings Program’s indoor air quality solutions, offers a quiet-operating, MERV 15 measure of efficiency for residential air filters. In addition, it’s ideal for applications where the furnace air handler is not easily accessed by the homeowner. Minimal maintenance is required, including filter cartridge replacement and occasional inspection/brush cleaning of the ionization panel. Plus, the Infinity return air purifier is installed inside the living space, allowing for convenient and easy filter cartridge replacement.

“Americans spend an average of 90% of their time indoors, where concentrations of some pollutants are often two to five times higher than outside air,” said Holly Rhodes, Associate Director, Indoor Air Quality Products, Carrier. “Carrier is constantly striving to innovate and create products that will help families make their indoor environments healthier. The Infinity return air purifier provides an effective and low-maintenance option for homeowners to help inactivate airborne viruses and pathogens in their home as part of a mitigation strategy including hand washing, sanitization and other measures recommended by health experts.”

The Infinity return air purifier features Captures & Kills® technology, which treats the air using a three-step “Charge/Capture/Kill” process:

  • Step One: Charge – the purifier creates a “cloud” of electrically charged ions that attach themselves to airborne dust, pollen, viruses, germs and other particles as they pass through.
  • Step Two: Capture – the ionized particles are pulled toward an oppositely charged, pleated MERV 15 rated filter and captured at an extremely high rate.
  • Step Three: Kill – captured airborne microbes remain on the pleated filter instead of recirculating back into the home and are subjected to an intense electric field. There, 99% of select viruses and bacteria are inactivated.

To learn more about how the Infinity return air purifier works, visit carrier.com/purifier. And to learn how to help make homes healthier, please visit: corporate.carrier.com/healthyhomes.

About Carrier
Founded by the inventor of modern air conditioning, Carrier is a world leader in high-technology heating, air-conditioning and refrigeration solutions. Carrier experts provide sustainable solutions, integrating energy-efficient products, building controls and energy services for residential, commercial, retail, transport and food service customers. Carrier is a part of Carrier Global Corporation, a leading global provider of innovative healthy, safe, sustainable and intelligent building and cold chain solutions. For more information, visit carrier.com or follow @Carrier on Twitter.

1 The Infinity® air purifier has demonstrated effectiveness against the murine coronavirus, based on third-party testing (2020) showing a >99% inactivation, which is a virus similar to the human novel coronavirus (SARS-CoV-2) that causes COVID-19. Therefore, the Infinity air purifier can be expected to be effective against SARS-CoV-2 when used in accordance with its directions for use. Third-party testing (2012, 2007) also shows ≥99% inactivation for the type of virus that causes common colds, Streptococcus pyogenes and human influenza. Airborne particles must flow through your HVAC system and be trapped by the MERV 15 Infinity filter to be inactivated at 99%. Learn how it works at Carrier.com/purifier.

Infinity Return Air Purifier