Carrier Announces the 100th CO2OLtec® Integral System Installation in a SPAR Store in Switzerland
October 2, 2013
COLOGNE, Germany
Carrier Kältetechnik Schweiz has achieved a significant milestone with the installation of its 100th CO₂OLtec® Integral system in the Swiss SPAR supermarket in Schüpfen, which opened its doors in June 2013. Carrier’s CO₂OLtec Integral system, which uses the natural refrigerant CO₂, provides a fully integrated approach for the store’s refrigeration, space heating and cooling, ventilation and lighting needs. With this solution, the supermarket expects to achieve measurable gains in increasing energy efficiency, cutting its carbon footprint in half, and streamlining its operations with a single point of contact for purchasing, installation and service. Carrier, the world’s leader in high technology heating, air-conditioning and refrigeration solutions, is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp. (NYSE: UTX).
The CO₂OLtec Integral system leverages the waste heat created during the refrigeration process to cover the full heating requirements of the entire store, all year round, thus eliminating the need for a conventional gas heating system. During warm months, it provides cooling to ensure a pleasant shopping and working environment, and for even greater comfort, the cold air in front of refrigerated cabinets is drawn out and redistributed via the ventilation system.
The performance of this fully integrated concept is orchestrated by Carrier’s intelligent building management system, which controls the interactions among the various components of the commercial refrigeration, heating, cooling, ventilation and lighting systems, to achieve optimal levels of energy efficiency.
Mr. Elias Steiner, Head of Construction Department and Facility Management, SPAR Gruppe Schweiz, said, “The fully integrated planning and execution of the entire building services together with commercial refrigeration make clear sense, because commercial refrigeration in a supermarket is proportionally the largest refrigeration system, the largest waste heat generator and the largest energy consumer. The concept of bringing these all ‘under one roof’ and optimally harmonising the controls is a future-proof idea.”
Philippe Widemann, Managing Director, Carrier Kältetechnik Schweiz, stated, “With increasing market acceptance of our fully integrated solution for supermarkets, Carrier is pleased to count SPAR’s Schüpfen store as our 100th CO₂OLtec Integral customer. Our customer can now take advantage of demonstrated energy cost savings of up to 30 percent over the system’s lifecycle, along with the future-proof security that comes with using CO₂ as a refrigerant.”
Carrier has the right refrigerant solution for every application, but not every refrigerant is suitable for every application.
About Carrier
Carrier is the world’s leading provider of advanced technical solutions for heating, air conditioning and refrigeration engineering. Carrier offers sustainable solutions for energy-efficient products, building control engineering and energy services in the areas of residential buildings, commercial refrigeration, transport and food retailing. Founded by the inventor of modern climate technology, Carrier achieves, through technical innovation and ecological responsibility, a valuable contribution to the preservation of our environment. Carrier is part of UTC Climate, Controls & Security, a business division of United Technologies Corp. UTC is the world’s leading provider in the areas of aerospace industries and building services engineering. Visit www.carrier.com, for more information.
About SPAR Gruppe Schweiz
The SPAR Group is a Swiss family business based in Gossau SG. In 1989 the business acquired the SPAR license for the whole of Switzerland from SPAR International. 170 EUROSPAR supermarkets, SPAR convenience stores and SPAR express convenience stores along with eleven TopCC cash-and-carry stores for large-scale consumers belong to the SPAR Group. A third of the SPAR convenience stores are separate branches, the other two thirds are led by independent retailers as part of the franchising system. Independent maxi and further free retailers are likewise supplied by SPAR. The SPAR Group employs 2156 full-time employees – 308 of whom are trainees. In 2012 a turnover of 1,041 million Swiss francs was generated.
SPAR provides grocery supermarkets, a large range of fresh products and friendly and proficient personnel to the neighborhood. SPAR International has its head office in the Netherlands. SPAR provides a licensing system in 36 countries. SPAR is thus the largest voluntary chain of retail stores with around 12,000 supermarkets and a total turnover of 31 billion euros. “SPAR” means “Tanne” in Dutch and was founded in Holland in 1932.
Installation description:
CO2OLtec Integral system at Spar Store, Switzerland by Carrier
Carrier´s CO₂OLtec Integral solution at a SPAR store in Schüpfen, Switzerland combines refrigeration, heating, cooling, ventilation and lighting and aims to achieve up to 30 percent savings on energy costs and 50 percent reduction in the system´s carbon footprint, in comparison to a conventional R404A refrigeration and gas heating system.
Across the sales area of almost 400 sqm, all pieces of cooling and freezing equipment are powered by a transcritical CO₂ booster refrigeration system. Waste heat created during the refrigeration process is collected by the CO₂OLtec Integral outdoor unit and reused to deliver the necessary heating capacity for the sales, storage and staff areas for the whole store year round. This allows the store to completely eliminate a conventional heating gas boiler system and the local usage of fossil fuels.
The central CO₂OLtec Integral outdoor unit secures cooling of the store when needed, by preparing cold water and distributing it via the hydraulic systems to various consumer points, such as the central air handling unit.
An additional system feature exhausts the cold air from the space in front of the open multidecks, thus helping to eliminate the “cold aisle effect”, and redistributing the air at the required temperature level via the central air handling unit.
The efficiency of the fully integrated concept is determined primarily by the optimum interaction of the interfaces of various subsections and the intelligence of the higher-level building management system that ensures that the various systems are fully integrated and interact with one another with the best possible efficiency.
Many critical interfaces to technical building equipment could hereby be eliminated, since all system components of the commercial refrigeration, heating, cooling, ventilation and lighting as well as their installation and service are delivered from a single source, by Carrier.