New Carrier Transicold Vector™ 8500 Unit Sheds Pounds, Beefs Up Performance

Sep 17, 2013

ATHENS, Ga., U.S.

Significantly reduced weight, improved fuel economy and greater refrigeration capacity are a trio of advantages found in Carrier Transicold’s new Vector™ 8500 single-temperature hybrid trailer refrigeration unit. Carrier Transicold helps improve global transport and shipping temperature control with a complete line of equipment for refrigerated trucks, trailers and containers, and is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp. (NYSE: UTX).

With the Vector 8500 unit, Carrier Transicold introduces the first fully hermetic electric scroll compressor used in a North American trailer refrigeration unit. Proven efficient and reliable in Carrier Transicold refrigerated marine container systems, the scroll compressor has 70 percent fewer moving parts and is 200 pounds lighter than a traditional reciprocating compressor.

As with other 2013 Carrier Transicold models, the Vector 8500 unit incorporates Carrier Transicold’s ecoFORWARD™ technologies, which boost performance while providing compliance with 2013 Tier 4 emissions requirements from the U.S. Environmental Protection Agency.

“The expression ‘work smarter not harder,’ truly applies to our systems with ecoFORWARD technologies,” said Bertrand Gueguen, president, Global Truck/Trailer, Carrier Transicold. “Innovative improvements in efficiency allow individual components, such as the engine, to use less energy while producing greater results – all in a system configuration that remains familiar to owners of prior Vector equipment.”

Added David Kiefer, director of Marketing and Product Management, “While Carrier Transicold’s legacy Vector units are highly efficient, the new ultra-efficient Vector 8500 achieves 5 to 30 percent more BTUs of cooling per gallon of fuel at AHRI rating conditions.”

The Vector platform’s signature E-Drive™ all-electric refrigeration technology means refrigeration and heating operations are 100 percent electric, powered over the road by an on-board generator driven by the unit’s diesel engine. Additionally, electric standby capability is built-in, allowing haulers to tap into electric power supplies to run the system when parked, providing quiet, emissions-free refrigeration performance that can reduce operating costs by up to 70 percent compared to diesel operations, while conserving fuel for the highway.

“Vector systems provide the dual benefits of reduced maintenance requirements and higher system reliability because overall they are less complex than conventional mechanical systems or competitive partially-electric systems,” Kiefer said.

A core component of Carrier’s exclusive ecoFORWARD technologies is a 2.2-liter engine that has been made smarter through the use of sensors and an electronic control module that communicates with Carrier’s APX™ control system to optimize performance. The sophisticated, yet easy to use APX control system is now standard with Carrier’s 2013 models.

Compared to the unit it succeeds, the new Vector 8500:
• Weighs 210 pounds less, a 10 percent weight savings, which also makes the Vector 8500 unit between 3 to 15 percent lighter than competitive units designed for 2013 EPA Tier 4 compliance
• Provides up to 4 percent higher cooling capacity – 60,000 BTU at 35 degrees F and 24,000 BTU at -20 degrees F
• Consumes up to 26 percent less fuel over a full range of operating conditions
• Reduces engine runtime by up to 14 percent, resulting in improvements in durability and longevity as a result of more lightly loaded components

In start/stop mode, the greater capacity and higher efficiency also help the Vector 8500 achieve setpoint faster, enabling the engine to shut off sooner, ultimately reducing engine run hours and runtime-based maintenance expense.

Using 20 percent less engine power than previous Carrier Transicold models, the Vector 8500 unit’s engine is certified for “evergreen” compliance with the 2013 EPA Tier 4 standard for engines less than 25 horsepower. For fleets operating in California beyond seven years, the Vector platform’s standard electric standby capability provides an in-use compliance option for the California Air Resource Board (CARB). Carrier Transicold is also developing an optional engine emissions system that further reduces engine emissions and provides a future CARB in-use compliance Verified Diesel Emissions Control (VDEC) strategy.

For more information about the Vector 8500 single-temperature trailer unit from Carrier Transicold, turn to the experts within the Carrier Transicold dealer network, visit www.carrier.com/ecoforward or follow Carrier on Twitter: @carriergreen.

About Carrier Transicold
Carrier Transicold helps improve transport and shipping temperature control with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 40 years, Carrier Transicold has been an industry leader, providing customers around the world with the most advanced, energy efficient and environmentally sound container refrigeration systems and generator sets, direct-drive and diesel truck units and trailer refrigeration systems. Carrier Transicold is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. Visit www.transicold.carrier.com for more information. Follow Carrier on Twitter: @carriergreen.

Carrier Transicold, Global Media Contact Jon Shaw Send An Inquiry