Carrier Transicold Releases TRU-Tech™ and TRU-View™ Software For Easy Management of Transport Refrigeration Units

Jan 14, 2014

ATHENS, Ga., United States

Custom configuration of transport refrigeration unit (TRU) settings and operations analysis is now easier than ever with Carrier Transicold’s new TRU-Tech™ and TRU-View™ computer applications. Carrier Transicold helps improve global transport and shipping of temperature-controlled cargoes with a complete line of equipment for refrigerated trucks, trailers and containers, and is a part of UTC Building & Industrial Systems, a unit of United Technologies Corp. (NYSE: UTX).

Successors to Carrier Transicold’s popular ReeferManager™ software, the TRU-Tech and TRU-View programs feature a simplified interface with icons and quick links for faster, easier navigation.

TRU-Tech refrigeration unit management software is a complete solution for refrigeration data management, including setting operational parameters and conducting diagnostic functions. TRU-Tech comes with TRU-View refrigeration data analysis software, which provides convenient insight into system performance. TRU-View is also available as a stand-alone application for data analysis, without the unit set-up and diagnostic capabilities of TRU-Tech.

Compatible with the latest Windows® operating systems, the new programs are designed for use with all Vector™, X4™, X2™ and X-Series trailer units, as well as Carrier Transicold’s Supra™ truck units.

“Today’s transport refrigeration units – or TRUs – have a wider array of settings, enabling a higher degree of control sophistication,” said Mark Fragnito, product, manager, electronics, Carrier Transicold. “While each refrigeration unit controller can be manually configured at the unit’s keypad, TRU-Tech software provides a faster and easier way to create multiple settings using either a Windows-based computer or tablet. The settings can then be loaded into a single unit or an entire fleet.”

TRU-Tech software’s intuitive screen layout makes it easy to create error-free IntelliSet™ commodity profiles. IntelliSet profiles, which are used with Carrier Transicold APX™ and Advance™ controls, direct the unit microprocessor to automatically adjust operating parameters for a particular load when the driver selects a commodity or customer name from a list on the control display. Fleets can use IntelliSet profiles to help maintain the optimum balance between temperature control and fuel economy, while also helping to eliminate the chance of driver errors.

TRU-Tech software can also be used by technicians to monitor system parameters, such as sensor inputs and other vital data that may be downloaded for tracking, performance evaluation, record keeping, or analytics. The TRU-View component can generate graphic reports, showing specific TRU system performance over time, and data can be exported into Excel® spreadsheets or PDFs for easy sharing.

With both programs, data transfers can be handled easily via a special USB jump drive with the APX control system or via PC cards with the Advance microprocessor. For telematics-enabled refrigeration units, data transfers can be handled wirelessly.

For more information on TRU-Tech and TRU-View software, turn to the experts within the Carrier Transicold dealer network or visit www.transicold.carrier.com.

About Carrier Transicold
Carrier Transicold helps improve transport and shipping of temperature-controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 40 years, Carrier Transicold has been an industry leader, providing customers around the world with the most advanced, energy efficient and environmentally sound container refrigeration systems and generator sets, direct-drive and diesel truck units and trailer refrigeration systems. Carrier Transicold is a part of UTC Building & Industrial Systems, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. Visit www.transicold.carrier.com for more information. Follow Carrier on Twitter: @CarrierGreen.

Carrier Transicold, Global Media Contact Jon Shaw Send An Inquiry