Carrier Transicold Introduces New Features on its Supra™ Range

Nov 19, 2015

Rouen, France

Learn more about sustainable cold chain solutions at the Solutrans Show, stand 4M196, hall 4, 17 November – 21 November 2015

Solutrans Supra

Carrier Transicold will present a series of new equipment and options for its Supra™ range of truck refrigeration units at the Solutrans show. The upgrades are designed to further enhance the customer experience and increase opportunities for customers to improve environmental sustainability. Carrier Transicold, operating in France as Carrier Transicold France, is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp. (NYSE: UTX).

Fleets will benefit from a new cab command panel, which has been designed to fit the standard DIN format used for audio head units in the automotive sector – making installation simpler. It offers improved ergonomics through larger buttons and features a large white backlit screen enabling the driver to see key information at a glance. The revised cab command panel will be introduced during 2016 as standard for all new Supra mono- and multi-temperature units, and can be retrofitted to existing Supra units in service.

Customers will also have the option to specify Supra units with a new package to reduce emissions. The package comprises three key elements, including a low emission diesel engine to reduce particulate matter by up to 50 percent versus the standard engine, plus the use of new R-452A refrigerant. R-452A has the same cooling capacity, fuel efficiency, reliability and refrigerant charge as the standard R-404A, but offers a 45 percent reduction in Global Warming Potential (GWP). Completing the package offering is Carrier’s Silent option kit, which helps to reduce unit noise emissions.

For fleets wanting to minimise noise emissions further, the “Pure” pack can be specified on the ultra-low noise, PIEK-compliant Supra City units, which operate below 60 decibels and are ideal for night-time deliveries in urban areas.

Carrier Transicold will also launch a new evaporator range for its Supra and Vector™ ranges at the Solutrans show. Suitable for multi-temperature applications, the evaporators feature new styling and are available in four widths ranging from 700 millimeters to 2,200 millimeters. A new defrost operation and improved water drain eliminates the risk of water splashing onto the cargo being transported. The new evaporators can be installed quickly and easily, with a fast dismounting system to aid maintenance and repair.

The Supra range forms a key part of the Carrier Transicold product line-up and has offered proven performance and reliability since the first generation Supra units were introduced in 1995.

For more information on Carrier Transicold products and services, visit our website www.carriertransicold.fr or follow us on Twitter @SmartColdChain.

About Carrier Transicold
Carrier Transicold helps improve transport and shipping of temperature controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 40 years, Carrier Transicold has been an industry leader, providing customers around the world with the most advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. For more information, visit www.transicold.carrier.com. Follow Carrier on Twitter: @SmartColdChain.