3 Distribution Ltd Gains Remote Control with Carrier Transicold’s Foretrack™ Upgrade

WARRINGTON, England -

3 Distribution Ltd can now remotely alter the set point of its Carrier Transicold transport refrigeration units, helping guarantee cold chain integrity for its customers. The King’s Lynn-based haulier is one of the first customers in the UK to use Carrier Transicold’s upgraded Foretrack™ proprietary tracking, telematics and fleet management system, after providing valuable feedback during the system’s development and trialling the next-generation software ahead of its official rollout. Carrier Transicold, which operates in the UK as Carrier Transicold (UK) Limited, is a part of the UTC Climate, Controls & Security, a unit of United Technologies Corp. (NYSE:UTX).

Now available for download as a mobile app on both iOS and Android devices, the upgraded version of Foretrack features two-way communication from a connected device anywhere in the world. This provides 3 Distribution with a wealth of new functionality, including the ability to remotely alter the set point or operation mode as well as initiate defrosts and pre-trip checks, and clear alarms.

"The ability to constantly monitor our multi-temperature fridges and change the settings while they’re on the road has proved invaluable when guaranteeing cold chain integrity for our customers,” said Patrick Finch, managing director, 3 Distribution Ltd. “In the unlikely event the fridge hasn’t been reset or is at an incorrect temperature, we can log in and save a small human error from potentially spoiling a load.”

The latest version of Foretrack also features an enhanced voice alert and escalation mechanism, which auto-escalates alarms to a higher level if they aren’t dealt with quickly by the first person in the chain. Fuel levels can also be closely monitored, helping to defend against fuel theft.

Established in July 2007, 3 Distribution operates a fleet of 34 Chereau, Gray & Adams and Schmitz Cargobull trailers and three rigid trucks, and has operated a 100 per cent Carrier-cooled fleet for a decade. Each vehicle covers around 65,000 miles each year, transporting a mix of ambient, chilled and frozen foods across the UK, seven days a week.

For more information on Carrier Transicold and its products and services, visit www.carriertransicold.co.uk. Follow Carrier Transicold on Twitter: @SmartColdChain.

About Carrier Transicold
Carrier Transicold helps improve transport and shipping of temperature controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 45 years, Carrier Transicold has been an industry leader, providing customers around the world with advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. For more information, visit www.carriertransicold.co.uk. Follow Carrier on Twitter: @SmartColdChain.

3 Distribution Ltd can now remotely alter the set point of its Carrier Transicold transport refrigeration units, using upgraded Foretrack™ software.

The haulier is one of the first customers in the UK to use Carrier Transicold's upgraded Foretrack™ proprietary tracking, telematics and fleet management system.