Carrier Expands WeatherExpert™ Rooftop Line to 150 Tons

Aug 19, 2013

SYRACUSE, N.Y., U.S.

Carrier’s highest efficiency commercial rooftop line, the WeatherExpert™ Series, now includes six new models from 75- to 150-tons, for a total model line-up ranging from 3- to 150-ton units. The WeatherExpert line boasts industry-leading Integrated Energy Efficiency Ratio (IEER) ratings up to 21.0 that exceed the Consortium of Energy Efficiency (CEE) tier II criteria, which many utilities use for rebates. They also meet or exceed all current ASHRAE 90.1-2010 and Energy Star® energy requirements, with some models exceeding standards by more than 84 percent. Carrier, the world’s leader in high technology heating, air-conditioning and refrigeration solutions, is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp. (NYSE: UTX).

Carrier collaborated with customers to design the latest WeatherExpert rooftop models, which represent the largest sizes the company has ever offered. The “ground-up design” provides valued flexibility and efficiencies needed for today’s and tomorrow’s markets, presenting customers with a lower cost-of-total-ownership product option.

“It’s a testament to our design team, who worked closely with our customers, that the WeatherExpert rooftop units won recognition in the Cooling Category for the 2013 AHR Expo Innovation Awards Competition,” stated Greg Alcorn, vice president, commercial sales and marketing, Carrier. “With the addition of these six models, Carrier has its most comprehensive and efficient rooftop lines ever, with units ranging from 3 to 150 tons.”

Similar to other models in the Carrier Weather Series line, the WeatherExpert 75- to 150-ton units were designed to maintain product familiarity by taking advantage of common parts from existing Carrier rooftop designs. With six sizes between 75 and 150 tons, customers are able to configure the equipment to be specifically tailored to their exact application, while enjoying convenient access to product support from Carrier experts in their market both during and after installation. 

The new WeatherExpert 75- to 150-ton models feature a double- wall foam panel cabinet design with hinged “man-sized” access panels. Customers can select between the standard airfoil supply fan or the optional high static airfoil supply fan as a solution to the static pressure necessary for today’s complex building applications and highly featured units. Units are also available in dedicated vertical, horizontal and mixed supply/return airflow configurations for constant volume (CV), staged air volume (SAV) or variable air volume (VAV) applications. Each WeatherExpert model comes with the ComfortLink DDC (direct digital control) communicating control system and hermetic staging scroll compressors on refrigerant circuits controlled via Electronic Expansion Valves (EXV).

In addition, the WeatherExpert 75- to 150-ton units are available in gas/electric, electric/electric and cooling only applications that are offered with a range of pre-engineered and certified factory options, such as the Humidi-MiZer® adaptive dehumidification system, service valves, disconnect switches and much more.

“The WeatherExpert units deliver optimal comfort and energy savings at both full- and part-load conditions,” added Alcorn. “Our control logic operates the multi-stage system to provide what our customers are looking for – smart, efficient operation with comfort control.”

All WeatherExpert units feature Puron® refrigerant (R-410A), provide easy access for routine maintenance, are supported by Carrier’s eDesign Suite and integrate with Carrier’s i-Vu® system controls.

For more information on the performance, innovation and reliability of Carrier WeatherExpert commercial rooftops, visit Carrier.com. Follow Carrier on Twitter: @CarrierGreen.

ABOUT CARRIER

Carrier is the world’s leader in high technology heating, air-conditioning and refrigeration solutions. Carrier experts provide sustainable solutions, integrating energy-efficient products, building controls, and energy services for residential, commercial, retail, transport and foodservice customers. Founded by the inventor of modern air conditioning, Carrier improves the world around us through engineered innovation and environmental stewardship. Carrier is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. Visit www.carrier.com for more information.

Media Contact Jeremy Riffle Send An Inquiry