Carrier Announces EnergyX® Energy Recovery System for 75-150-Ton WeatherExpert™ Rooftop Units

Jan 28, 2015

CHICAGO

Carrier is proud to announce the addition of the EnergyX factory integrated, energy recovery ventilator (ERV) option to the WeatherExpert 48/50N series of large, 75- to 150-ton rooftop units. Carrier, a world leader in high-technology heating, ventilating and air-conditioning solutions, is a part of UTC Building & Industrial Systems, a unit of United Technologies Corp. (NYSE: UTX).

Carrier’s EnergyX energy recovery system is a factory integrated and tested ERV that provides an AHRI 1060-certified rotary energy wheel. EnergyX holds and transfers energy from the exhaust airstream to improve energy savings and increase ventilation. Using building exhaust air as a heat source, it has been designed to pre-condition the outside air prior to entering the rooftop unit. The system provides latent and sensible energy exchange between the outside ventilation air and the building exhaust air. Compliant to ASHRAE Standard 90.1, this preconditioning of air allows for higher operating efficiencies, increased comfort control, and potential downsizing of the base rooftop unit while also meeting ASHRAE Standard 62.1 ventilation requirements.

EnergyX was previously available on 3- to 25-ton WeatherMaster® rooftop units. Adding the EnergyX option to any Carrier WeatherExpert 48/50N series rooftop unit can improve indoor air quality and decrease operating costs.

“Carrier recognizes customers’ desire for improved indoor air quality and energy savings, and this expansion represents our continued commitment to serve both needs,” said Greg Alcorn, vice president, commercial sales and marketing, Carrier. “Carrier will continue to innovate to provide our valued customers with the most reliable and efficient commercial heating and cooling products.”

For more information, visit www.commercial.carrier.com or follow @CarrierGreen on Twitter.

About Carrier
Founded by the inventor of modern air conditioning, Carrier is the world’s leader in high-technology heating, air-conditioning and refrigeration solutions. Carrier experts provide sustainable solutions, integrating energy-efficient products, building controls and energy services for residential, commercial, retail, transport and food service customers. Carrier is a part of UTC Building & Industrial Systems, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. For more information, visit www.carrier.com or follow @CarrierGreen on Twitter.

Carrier Media Contact Bryan Mitchell Send An Inquiry