Sustainable, Forward Thinking: Carrier Transicold Develops Ultra-Efficient Trailer Refrigeration Technology

March 21, 2012

LOUISVILLE, KY, US

Helping the North American refrigerated transport industry improve efficiency and sustainability, Carrier Transicold presented its next generation trailer refrigeration technology today at the 2012 Mid-America Trucking Show in Louisville. The ultra-efficient system is designed to consume less fuel, perform quieter and deliver improved cooling performance, all while running cleaner than any prior Carrier Transicold trailer unit. Carrier Transicold helps improve global transport and shipping temperature control with a complete line of equipment for refrigerated trucks, trailers and containers, and is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp. (NYSE: UTX).

Carrier Transicold’s next generation technology also provides solutions for refrigerated transporters facing upcoming changes to the U.S. Environmental Protection Agency emissions standards in 2013, as well as California Air Resources Board (CARB) emissions requirements.

“A major milestone in our continuous product development, this next generation trailer technology boosts performance and efficiency and intelligently coordinates refrigeration with a smarter engine,” said David Appel, president, Carrier Transicold. “The efficiency gains allow us to significantly reduce engine power, enabling better fuel economy.”

Carrier Transicold’s new technology reduces engine power by 18 to 20 percent and enables up to 20 percent lower fuel consumption, compared to previous models over a full range of operating conditions. It will be applied to Carrier Transicold’s Vector™ hybrid diesel-electric and the X2™ series of belt-driven units with slight variations between each, such as a reduction in weight for Vector units.

“Reducing emissions was one of the main goals in our development process,” said David Kiefer, director of marketing and product management, Carrier Transicold. “We challenged ourselves to evaluate our systems holistically, while considering our customers’ long-term needs beyond immediate compliance requirements. The result is a fusion of new innovations with proven technologies from our successful platforms.”

A common element of the technology is a 2.2-liter diesel engine that is based on Carrier Transicold’s established engine line and is made smarter with the addition of sensors and an electronic control module. Common to both platforms will be implementation of the APX control system with new power-management algorithms and intelligent refrigeration system control; improvements to the condenser, heat exchanger and fan designs for greater efficiency and sound reduction; and a new custom-designed Engine Emissions System (EES) for unprecedented emissions reduction. “This technology enhances Carrier Transicold’s existing innovative and reliable designs in a way that achieves both greater efficiency and higher performance,” Kiefer said.

Beyond fuel savings, other benefits of this next generation technology include:

  • Improved cooling capacity for most applications, resulting in up to 20 percent faster pulldown
  • Reliable unit operation in even in hotter ambient conditions
  • Up to a 20 percent reduction in greenhouse gas emissions, commensurate with the reduced fuel consumption
  • Improvements in durability and longevity due to more lightly loaded components running at lower speeds

This technology also responds to new, more stringent EPA tests that, starting in 2013 will require emissions performance over an even broader range of operating parameters than in the past. Its EES is designed to reduce particulate emissions beyond what is required for EPA Tier 4 compliance and far exceeds the requirements of CARB’s applicable ultra-low diesel emission requirement.

Additional design changes and benefits will be unique to the platforms. For example, compressor and generator design modifications will be made to improve efficiency. which is also expected to significantly reduce the weight of Vector hybrid units. Regarding the X2 series, units will require 24 percent less refrigerant, reducing another potential source of greenhouse gases.

Units featuring the next generation technology will be available in limited quantities by the end of the year, and fully available in 2013. For more information about Carrier Transicold trailer refrigeration units, turn to the experts within the Carrier Transicold dealer network or visit www.trucktrailer.carrier.com.

About Carrier Transicold
Carrier Transicold helps improve transport and shipping temperature control with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 40 years, Carrier Transicold has been an industry leader, providing customers around the world with the most advanced, energy efficient and environmentally sound container refrigeration systems and generator sets, direct-drive and diesel truck units and trailer refrigeration systems. Carrier Transicold is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. Visit www.transicold.carrier.com for more information.

Media Contact

Media Contact Thomas  Cunningham 412-486-0076
cunningthomas@yahoo.com