New EcoFORWARD™ Technologies from Carrier Transicold Add Up to Ultra-Efficient Transport Refrigeration Units

June 11, 2012

ATHENS, Ga., US

“EcoFORWARD™ technologies” is the new name behind the ultra-efficient transport refrigeration units and generator sets designed by Carrier Transicold for compliance with U.S. Environmental Protection Agency diesel emissions standards, which change in 2013. Carrier Transicold helps improve global transport and shipping temperature control with a complete line of equipment for refrigerated trucks, trailers and containers, and is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp. (NYSE: UTX).

Transport refrigeration systems with ecoFORWARD technologies will consume significantly less fuel, operate quieter and deliver improved performance, all while running cleaner than the models they will replace. Carrier Transicold has also launched an Internet microsite to help customers learn about the new technologies, www.carrier.com/ecoforward.

“EcoFORWARD technologies are an important milestone in Carrier Transicold’s continuous product development for transport refrigeration customers,” said David Appel, president, Carrier Transicold. “These innovative technologies include a range of forward-thinking enhancements that will boost performance and efficiency and intelligently coordinate refrigeration with a smarter engine. The efficiency gains allow us to significantly reduce engine power, enabling better fuel economy to help our North American refrigerated transport customers move their own businesses forward in more sustainable ways.”

Common to systems with ecoFORWARD technologies are 2.2-liter diesel engines based on Carrier Transicold’s established engine line and made smarter with the addition of sensors and electronic control modules. Performance gains from the application of ecoFORWARD technologies mean that engine power can be reduced by 18 to 20 percent, putting them within the scope of EPA’s Tier 4 standard for nonhighway engines rated at 11 to 25 horsepower. For trailer refrigeration, efficiency improvements result in a 5 to 20 percent reduction in fuel consumption compared to previous models, over a full range of operating conditions.

A new custom-designed engine emissions system (EES) adds unprecedented emissions reduction and compliance with the California Air Resources Board ultra-low emissions standard. EcoFORWARD technologies are being applied to Carrier Transicold’s trailer refrigeration platforms, both the belt-driven units and the Vector™ hybrid diesel-electric units, as well as the PowerLINE™ generator sets used with container refrigeration systems for overland intermodal applications.

Units featuring the ecoFORWARD technologies will be available in limited quantities by the end of the year and fully available in 2013. For more information about ecoFORWARD technologies from Carrier Transicold, visit www.carrier.com/ecoforward.

About Carrier Transicold
Carrier Transicold helps improve transport and shipping temperature control with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 40 years, Carrier Transicold has been an industry leader, providing customers around the world with the most advanced, energy efficient and environmentally sound container refrigeration systems and generator sets, direct-drive and diesel truck units and trailer refrigeration systems. Carrier Transicold is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. Visit www.transicold.carrier.com for more information.

Media Contact

Carrier Transicold, Global Media Contact Jon Shaw Send An Inquiry