New Carrier® Performance™ 80 Gas Furnace Leverages ComfortHeat™ Technology for Advanced Comfort

Sep 5, 2013

INDIANAPOLIS, U.S.

Carrier announces the release of the Performance 80 58CTW two-stage, variable-speed gas furnace, which offers unmatched comfort in its class with ComfortHeat technology and up to 80% Annual Fuel Utilization Efficiency (AFUE). Carrier, the world’s leader in high technology heating, air-conditioning and refrigeration solutions, is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp. (NYSE: UTX).

The Performance 80 boasts numerous advantages including ComfortHeat technology, which offers decreased sound levels, longer cycles, fewer temperature swings between cycles and a consistent temperature between rooms. Its exclusive, intelligent control adapts to the heating needs of the home by automatically adjusting high- and low-heat times to maximize comfort.

In addition, the Performance 80 delivers two-stage heating with single-stage thermostat-patented Adaptive Control Technology. The Performance 80 also comes equipped with the QuietTech™ system, providing low operating sound, SmartEvap™ technology moisture-control function and ComfortFan™ technology, which allows homeowners to adjust the constant fan speed from the thermostat.

“The new Performance 80 gas furnace provides a solid entry point into Carrier’s Performance tiered furnaces,” said Tom Archer, senior product manager, Carrier. “While this product offers homeowners many benefits, I believe the most significant is the way in which the advanced technologies utilized by this single unit work together to create an unparalleled level of comfort in the home.”

Homeowners also have multiple installation options due to the Performance 80’s four-way multipoise design with 13 vent applications. Plus, its variable-speed electronically commutated motor (ECM) motor allows for efficient operation all year long in heating, cooling and continuous fan operation.

Visit www.carrier.com to learn more. Follow Carrier on Twitter @CarrierGreen.

ABOUT CARRIER

Carrier is the world’s leader in high technology heating, air-conditioning and refrigeration solutions. Carrier experts provide sustainable solutions, integrating energy-efficient products, building controls, and energy services for residential, commercial, retail, transport and foodservice customers. Founded by the inventor of modern air conditioning, Carrier improves the world around us through engineered innovation and environmental stewardship. Carrier is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. Visit www.carrier.com for more information.

Media Contact

Media Contact Jeremy Riffle Send An Inquiry