Carrier Transicold UK Offers Advice on New F-Gas Legislation at CV Show - Stand 3D110, Hall 3, Commercial Vehicle Show, NEC, Birmingham, 14 - 16 April 2015

April 14, 2015

WARRINGTON, England

Carrier Transicold UK will provide advice to temperature controlled vehicle operators on the new EU517/2014 F-Gas regulation at the 2015 Commercial Vehicle Show. Carrier Transicold, which operates in the UK as Carrier Transicold UK, helps improve global transport and shipping temperature control with a complete line of equipment for refrigerated trucks, trailers and containers, and is a part of UTC Building & Industrial Systems, a unit of United Technologies Corp. (NYSE: UTX).

The new F-gas regulation, which went into effect on January 1, 2015, impacts the use and maintenance of transport refrigeration equipment containing hydrofluorocarbons (HFCs) on vehicles plated above 3.5 tonnes, including trailers. This includes a planned phase-down of HFCs, to reduce the quantity that can be sold in the EU by 79 percent by 2030. This will have an effect on availability of HFCs. There is also a new requirement for transport refrigeration for mandatory leak checks, record keeping and the use of trained technicians holding an F-Gas handling certificate for all refrigerant handling operations. 

"These new regulations represent some of the biggest changes affecting our industry over the past decade," said Andy Wainwright, service director, Carrier Transicold UK. "Our in-house team of experts will be at our stand to answer any questions customers may have and to help them identify the steps they can take to ensure compliance."

In Europe, Carrier Transicold is actively working towards replacing current HFC refrigerants with natural refrigerant CO2 (R744), which has a global warming potential (GWP) of 1. In the meantime, Carrier Transicold has announced at the CV Show that it will offer R452A as an optional alternative to the existing R404A refrigerant. R452A has the same cooling capacity, fuel efficiency, reliability and refrigerant charge as R404A, but offers a 45 per cent GWP reduction.

Carrier will introduce this new refrigerant over the second and third quarters of 2015 as an option across its Vector™ trailer refrigeration and Supra truck refrigeration product ranges. Customers will also have the option to convert existing units to operate on R452A. These new options are part of Carrier's commitment to serving customers with the right refrigeration solution for every application, while not every application may have the same refrigerant solution.

Carrier Transicold UK can also directly support customers in meeting the F-gas legislation through its newly launched everCOLD™ flexible maintenance package, which includes all required maintenance and system leak checks performed by F-Gas certified engineers in accordance with EU517/2014.

Carrier Transicold's exhibition stand also features an exclusive "innovation lab," offering visitors greater insight into the brand's vision for the use of natural refrigerants in future light commercial vehicle, truck and trailer products, which will help to further sustainability in the cold chain.

For more information on Carrier Transicold and its products and services, visit www.transicold.carrier.com or follow @CarrierGreen on Twitter.

About Carrier Transicold

Carrier Transicold helps improve transport and shipping of temperature controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 40 years, Carrier Transicold has been an industry leader, providing customers around the world with the most advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of UTC Building & Industrial Systems, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. For more information, visit www.transicold.carrier.com, or follow Carrier on Twitter: @CarrierGreen.

Media Contact

For Carrier Transicold Media Contact James  Keeler Send An Inquiry