Carrier Transicold Introduces CARB Level 3+ Verified Emissions System for Latest X4™ and Vector™ Series Trailer Refrigeration Units

Dec 10, 2013

Athens, Ga.

The new optional engine emissions system (EES) from Carrier Transicold, capable of reducing diesel particulate mass from trailer refrigeration unit exhaust by more than 98 percent, has received conditional verification from the California Air Resources Board (CARB). Carrier Transicold helps improve global transport and shipping of temperature-controlled cargoes with a complete line of equipment for refrigerated trucks, trailers and containers, and is a part of UTC Building & Industrial Systems, a unit of United Technologies Corp. (NYSE: UTX).

The Carrier Transicold EES is the first OEM-developed CARB level 3+ verified diesel emissions control (VDEC) device for trailer refrigeration units that can be included with initial purchase or added later for users who do not initially require it. A Level 3+ VDEC device reduces particulate emissions in accordance with CARB’s ultra-low emissions requirement for transport refrigeration units, also known as ULETRU, while also reducing nitrogen oxides.

“Carrier Transicold’s latest trailer refrigeration unit engines are already certified for ‘evergreen’ compliance with the 2013 EPA Tier 4 standard for engines less than 25 horsepower, allowing for indefinite use throughout North America, except in California,” said David Kiefer, director of marketing and product management, Carrier Transicold. “In California, CARB uniquely requires that a VDEC strategy be applied to units in this horsepower class for use in the state beyond the initial seven years.”

“CARB conditional verification validates the operation and effectiveness of the EES in Carrier’s 2013 Tier 4 refrigeration units,” Kiefer said. “This is a major milestone. It is the first and biggest step toward offering a broader array of CARB-compliant options to our customers.”

The EES is conditionally verified for use with Carrier Transicold’s new Tier 4-compliant designs, which include the X4™ Series single-temperature models 7500 and 7300, and the hybrid Vector™ 8500 single-temperature and Vector 8600MT multi-temperature units. In the current phase of the verification process, these Carrier Transicold units may be factory-equipped with the EES, and the EES can be installed on previously purchased units with up to 3,000 hours of engine operation.

“In accordance with CARB protocols, testing on aged trailer unit engines will continue into 2014 to verify EES performance on engines with far more hours of service, so as to eliminate the 3,000-hour provision,” Kiefer said.

Although trailer refrigeration units can be specified with the EES at the time of initial purchase, Carrier Transicold designed the system for ease of installation as a retrofit, since many users will not require it immediately.

For more information about the Carrier Transicold engine emissions system, turn to the experts within the Carrier Transicold dealer network or visit www.carrier.com/ecoforward.

About Carrier Transicold

Carrier Transicold helps improve transport and shipping of temperature-controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 40 years, Carrier Transicold has been an industry leader, providing customers around the world with the most advanced, energy efficient and environmentally sound container refrigeration systems and generator sets, direct-drive and diesel truck units and trailer refrigeration systems. Carrier Transicold is a part of UTC Building & Industrial Systems, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. Visit www.transicold.carrier.com for more information. Follow Carrier on Twitter: @CarrierGreen.


 

Media Contact

Carrier Transicold, Global Media Contact Jon Shaw Send An Inquiry