Carrier Transicold Bolsters Vector™ Trailer Refrigeration Unit Warranties

Oct 21, 2014

Athens, Ga.

Carrier Transicold has enhanced the warranty coverage for its Vector™ trailer refrigeration units, reflecting the series’ reputation for reliability. Carrier Transicold helps improve global transport and shipping of temperature-controlled cargoes with a complete line of equipment for refrigerated trucks, trailers and containers, and is a part of UTC Building & Industrial Systems, a unit of United Technologies Corp. (NYSE: UTX).

“Vector systems deliver dual benefits of reduced maintenance and higher system reliability because they are less complex than conventional mechanical systems and comparative semi-electric systems,” said Patrick McDonald, product manager – trailer, Carrier Transicold. “Our latest-generation Vector units build on this legacy, employing a fully hermetic electric scroll compressor with 70 percent fewer moving parts than a traditional reciprocating compressor.

“Eliminating mechanical parts, such as belts, pulleys, compressor shaft seals and vibrasorbers that require service and periodic replacement, reduces service requirements while improving reliability. In short, if it’s not there, it can’t break,” McDonald added. “It’s one of the key reasons we’re able to offer improved warranty coverage for our latest models.”

The warranties for the hybrid Vector 8500 and Vector 8600MT units now include 48-month/8,000-hour major component coverage for the engine, generator and compressor. This compares with 36-month/6,000-hour coverage on earlier models. Additionally, the APX™ control’s microprocessor and stepper valve modules are warrantied for 60 months/10,000 hours – one year longer than comparative control systems.

The Vector units continue to offer 12 months of unlimited coverage and 36-month/6,000-hour limited coverage for the entire unit. On the multi-temp Vector 8600MT, basic warranty coverage for the new, smarter remote evaporators has been extended to 36 months/6,000 hours, triple the warranty for prior remote evaporators.

The Vector 8100 engineless unit for stationary cold storage applications also now features improved warranty coverage, with the run-hours limit for 36-month basic coverage and 48-month major component coverage now extended to 10,000 hours.

The Vector platform’s signature E-Drive™ all-electric refrigeration technology means refrigeration and heating operations are 100 percent electric. All models can be plugged into an AC electrical supply when parked, providing full refrigeration capacity without engine noise, emissions or fuel consumption. Over the road, the 8500 and 8600MT units are powered by an on-board generator driven by the unit’s diesel engine, whereas the Vector 8100 unit does not require the engine-generator combination, because it is designed for stationary cold storage.

To learn more about the Vector platform, turn to the experts within the Carrier Transicold dealer network or visit www.carrier.com/ecoforward.

About Carrier Transicold
Carrier Transicold helps improve transport and shipping of temperature-controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 40 years, Carrier Transicold has been an industry leader, providing customers around the world with the most advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of UTC Building & Industrial Systems, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. Visit www.transicold.carrier.com for more information. Follow Carrier on Twitter: @CarrierGreen.

Media Contact

Carrier Transicold Jon Shaw Send An Inquiry