News

Carrier® Infinity® Heat Pump with Greenspeed™ Intelligence Receives Excellence in Design Award from appliance DESIGN Magazine

Aug 8, 2012

INDIANAPOLIS, US

Carrier, the world’s leader in high-technology heating, air-conditioning and refrigeration solutions, recently received a silver-level Excellence in Design award from appliance DESIGN magazine for its Carrier® Infinity® 20 heat pump with Greenspeed™ intelligence. This year marks the 25th year for the publication’s “Excellence in Design” awards. Products from 10 industry categories were evaluated, and the appliance DESIGN panel of judges selected the Carrier Infinity heat pump based on its innovation, simplicity, functionality, and other considerations, including optimized capabilities, environmental footprint and energy and cost savings. Carrier is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp. (NYSE: UTX).

Introduced in 2011, the Infinity heat pump with Greenspeed intelligence is the highest heating efficiency ducted, air source heat pump on the market with a Heating Seasonal Performance Factor (HSPF) efficiency rating up to 13. The Infinity heat pump delivers up to 69 percent higher heating efficiency in the three-ton size.

“At Carrier, we are continually enhancing the design of our products to be more energy efficient, reliable and easier to install and use, so it is an honor to receive an Excellence in Design award from appliance DESIGN magazine,” said John Gibbons, director, residential product strategy, Carrier. “Part of Carrier’s commitment to customers, contractors and the environment is designing systems, such as the Infinity heat pump with Greenspeed intelligence, that reduce overall energy use, consume fewer resources, and reduce our environmental footprint.”.

The Infinity 20 heat pump with Greenspeed intelligence was one of four HVAC products to receive the Excellence in Design designation from appliance DESIGN magazine.

“One of the many innovative features of the Infinity 20 heat pump is its ability to provide warmer air at the register when outdoor temperatures fall into the teens,” said Rob Lambert, product manager, Carrier. “Under similar conditions, standard heat pumps may deliver cooler air at the register when outdoor temperatures decline. The Infinity 20 heat pump with Greenspeed intelligence is one of the highest efficiency air source heat pumps built with consumer comfort in mind.”

With cooling efficiencies up to 20.5 Seasonal Energy Efficiency Ratio (SEER) and variable-speed compressor technology, this heat pump is also ideal for superior cooling and dehumidification in regions with warmer temperatures and high humidity.

For more information on the Infinity 20 heat pump with Greenspeed intelligence or additional Carrier products and services, call 1-800-CARRIER or go to www.carrier.com

About Carrier
Carrier is the world’s leader in high technology heating, air-conditioning and refrigeration solutions. Carrier experts provide sustainable solutions, integrating energy-efficient products, building controls, and energy services for residential, commercial, retail, transport and foodservice customers. Founded by the inventor of modern air conditioning, Carrier improves the world around us through engineered innovation and environmental stewardship. Carrier is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. Visit www.carrier.com for more information.

Media Contact

Carrier
Media Contact
Michelle Caldwell

Send An Inquiry